Part Number: TLK105L
Fault status: "The LED LINK indicator does not flash, and the upper computer cannot catch the data packet. Change the chip to a good board, and the fault is transferred. Change the chip to test OK at this position, and the fault…
Part Number: TLK105L Hello ,experts
Here is a TLK105L design
Connect it with PC,and use PC to ping it repeatly, after a long time , it would linkdown.
And at this time. MCU can not read the TLK105L register through MDIO interface any more.
The clock…
Part Number: TLK105L When using the tlk105l, we found that sometimes when powered on, the pfbout pin(pin 15) voltage will fall to about 0V, and the tlk105l does not work normally. At this time, even trigger reset pin it has no effect. What is the reason…
Part Number: TLK105L Other Parts Discussed in Thread: AM5718 , I am facing an issue with receive side of PRU ethernet (MII) used in our custom board Processor :: AM5718 PHY :: TLK105L interfaced to PRU1 of Processor I am using this interface for raw socket…
Part Number: TLK105L We have been seeing intermittent ethernet failures with one of our customers designs. Failure description is that the device doesn't power up correctly at times. Replacing the component always fixes the failure. Failure rate is…
Part Number: TMDSIDK437X Other Parts Discussed in Thread: TLK105L , TLK105 Hello.
1. I use NIMU_BasicExample_idkAM437x_armExampleproject. How can I read and write registers of TLK105L? For my project on my board, I will need my own settings. How can i do…
Hi Amy,
I haven't heard back from you in a while so I'll be closing this thread. Please open a new thread if you have further questions.
Thanks,
Lucas
All information in this correspondence and in any related correspondence is provided “as is…
Part Number: TLK106L Other Parts Discussed in Thread: TLK105L , , TLK106 I had a question on the TLK106L. I’m using the TLK106 PHY chip on my board .The datasheet is generic , and also applies for TLK105L.
The TLK106L works at maximum temperature of…
Other Parts Discussed in Thread: AM5728 Hello!
We would like to use a Microchip KSZ8041 PHY as the PHY for AM5728 icss_emac.
Will icss_emac work with this PHY?
Regards, Evgeny Rogozhkin
Part Number: TLK105L Other Parts Discussed in Thread: TLK105 Hi Team,
How do I configure the TLK105L for 100 Base-TX compliance testing? 1.The following script is for DP 83822. Should I run it like this? 2.Is the compliance test register (0x0027) the default…