Part Number: TLK106 Tool/software: A few questions: 1. What magnetics are required to work with the TLK106?
2. Is there any version of RJ45 with magnetics that has a breakout board that would work with the TLK106 for some benchtop testing?
3. Do you…
Part Number: TLK106 Other Parts Discussed in Thread: DP83822H I would like to implement a transformerless connection between Phy on a daughter card and a second phy on the main board it sits on. Distance between the two PHYs is less than 10cm.
Figure…
Part Number: TLK106 Other Parts Discussed in Thread: TLK110 Hello,
I am designing an Ethernet interface for a product that uses the TLK106 Ethernet PHY and I am having trouble understanding whether it supports transformer-less operation (with DC blocking…
Part Number: TLK106 Tool/software: Hello I am using a card from a 3rd supplier with an ethernet interface that uses the TLK106. The termination is already on this card, but the bias and caps for the center tap I need to put on my board.
I am interfacing…
Part Number: TLK106 Other Parts Discussed in Thread: , AM4377
Hello all,
I'm working with a device which uses 2x TLK106L and an AM4377 to run two EtherCAT ports. Due to the supply chain issues I am trying to use TLK106 instead of TLK106L. To my understanding…
Part Number: TLK106 Hello
We are using the TLK106I chip and we wanto to connect our microprocessor to it using the RMII interface.
For that purpose we have connected the lines of RMII and send the clock to MAC using two modalities: 1) the RX_CLK out…
Part Number: TLK106 Other Parts Discussed in Thread: DP83822I Hi, Our customer are using the TLK106RHBR in their projects before. They want to know if they can just replace the DP83822IRHBR instead of TLK106RHBR without Changes in Layout? Thanks, Ced…
Part Number: TLK106 Other Parts Discussed in Thread: DP83822H , DP83825I Good Evening,
We are experiencing an issue with some TLK106 PHYs when powering up at elevated temperatures. We have multiple boards, each with 7 PHYs installed, and are seeing…
Part Number: TLK106 Hi all Would you mind if we ask TLK106? We are sorry that we would like to confirm basic content. <Question1> Does FLP burst output from TD+/- port only? <Question2> Using Auto-MDIX function, does RD+/- port output FLP burst? In this…
Part Number: TLK106 Part number: TLK106RHBR
->This product is a communication IC, and it is not possible to test only the IC alone before production. After the production of our board is completed, the corresponding IC is replaced for the board that…