Part Number: TLK1501 we have been working on an optical communication with using two circuit board using TLK1501.
Transmission setting of TLK1501(sending) is established as TX_EN = '0' (IDLE) and transmits. Then monitored receiving data and RX_ER wit…
Part Number: TLK1501 Other Parts Discussed in Thread: TLK1221 Dears,
Now, i need a Deserialization to work with TLK1501(using as Serialization).
Because TLK1501 is Serialization and Deserialization integrated, its size is very big, we can't use it in…
Part Number: TLK1501EVM Other Parts Discussed in Thread: TLK1501 Hello,
I need a clarification about the use of the 10nF capacitor connected to ground between the two 50ohm termination resistors on the evaluation board of the TLK1501 (RX lines).
On the…
Part Number: TLK1501 Hi,
I am using the TLK1501 transceiver on my board which is interfacing with an FPGA. I was wondering if it is required to impedance match the RX and TX parallel data. The development kit impedances matches these lines to 50-ohms…
Part Number: TLK1501 My board has two tlk1501 and SFP Fiber channels , and I test internal loopback and Transmit / Receive through a single fiber for each of them separatley , both of them can work normally, including hot-plug function as well. But when…
Part Number: TLK1501
I'm trying to communicate with the FPGA on the other board. That doesn't work correctly. Look like I'm not in the sync state.
I generated a Xilinx IP core with the transceiver wizard (8b/10b, 1.25Gbps, no CB, no CC) for…
Part Number: TLK1501 Hi!
In the datasheet on TLK1501 it is said that the built-in 8b / 10b encoder automatically generates the sequence K28.5, D5.6 (K28.5, D16.2). According to the FibreChannel standard, this sequence should be K28.5 D21.4 (K28.5 D21…
Part Number: TLK1501 Hi Team,
Could you please send actual waveform of 59pin(DOUTTXN) and 60pin(DOUTTXP) if you have any data?
Because, we need a reference waveform.
Regards,
Kanemaru
Part Number: TLK1501EVM Other Parts Discussed in Thread: TLK1501 , Hello,
I asked this question over a year ago.
I have two TLK1501 EVM boards.
Each one has a high precision 62.5 MHZ oscillator with < 20ppm error. Frequency counter measures each one as…