Part Number: TLK3134 We have always used white for this product, but found that the 18+ product is black.
Could you please help to confirm the cause? Is there any inconsistency between color performance and parameters?
thank you.
Part Number: TLK3134 Hello,
I have found an application note to get rid of the FPGA and implementing Cameralink
Does anybody know whether we can convert SDI to HDMI with this chip?
The application note is below;
Thank You,
Regards,
Part Number: TLK3134 Hi Team, 1) I believe "PLOOP pin = high" leads to Figure 2-3 and "SLOOP pin = high" leads to Figure 2-2 without setting registers. Is my understanding correct? -----------------------------------------------------…
Part Number: TLK3134 Hi Team, My customer considers to use GMII mode. The Table 2-8 shows TXC(3:0) are assigned to TX_EN. On the other hand, Table 2-15 shows TXC(3:0) should be "0" when trasmitting Normal data. I couldn't understand why Table 2-15…
Part Number: TLK3134 Hello team,
I am trying to find a transceiver for the following interfaces that can drive cables over 4m:
XAUI interface at 3.125 Gbps
LVDS at 160 Mbps
I found the TLK3134 that can work with XAUI, and has built in de-emphasis, and there…
Other Parts Discussed in Thread: TLK3134 Hello,
I am trying to find drivers for the following interfaces that can drive cables over 3m:
XAUI interface at 3.125 Gbps
LVDS at 160 Mbps
I found the TLK3134 that can work with XAUI, and has built in de-emphasis…
Other Parts Discussed in Thread: TLK3134 , TLK10002 , TLK10034 , TLK10232 Mike
I found this thread on the forum and was hoping you could answer a similar question. We are looking into doing a new product that takes 10G KX4 which looks like it is the same…