Part Number: TLV1117 Customer wants TI's device(TLV1117) as second source to replace LDL1117, the LDL1117 link is LDL1117 , there are two demands:
1. Must can be pin to pin( SOT-223 )
2. Now they have find TLV1117 with SOT223 package, TLV1117's ESR…
Part Number: TLV1117 Hi Team,
There is a good new that we DIN TLV1117DCY!
And there have one thing need your support,
Please help check this SCH, THX
UP1K22R REV H_TLV1117.pdf
Part Number: TLV1117 Hi Team,
There is a good new that we could DIN TI product!
We are searching linear regulator IC, could for TLV1117CDCYR 12V transfer to 3.3V output. THX
Part Number: TLV1117 Other Parts Discussed in Thread: TL783 , LMS1585A , LM317 , LM340 , LM2904 , LM2937 Dear Specialists,
My customer is considering LDO of TO263-3 package.
I would be grateful if you could advise.
--
Regarding TO263-3 package, there are two…
Part Number: TLV1117 Hi Team,
My customer report TLV1117-50IDCYR abnormal output issue: Vout=~10V @Vin=12V. We did following 2 verification test:
1. Impedance between input and output pin: normal device=1.08M, issue device=1k
2. If we increase or decrease…
Part Number: TLV1117 Hello,
While testing parts for a customer I noticed that parts had mild abrasion marks on some of the leads.
Also when performing solderability testing I noticed that some of the leads did not take well to the solder. I am not very…
Part Number: TLV1117 Hi team,
we are using the TLV1117 for a supercap circuit. It is sourcing current into 4.4F caps.
can you please help verify that the device is producing about 4V and that the RC components are appropriate?
Thanks, Kevin
Part Number: TLV1117 Dear all,
Our customer is considering using TLV1117. According to the data sheet, it is described that an electrolytic capacitor having an ESR of 0.2Ω to 10Ω is used for stable operation as follows.
However, our customers…