Part Number: TLV1117 As to fixed version of TLV1117, whether it uses inner divider resistors or it has different inner reference?
if customer wants to use TLV1117-50 5V fixed output LDO as 12V output voltage LDO, how to realize it? could they add one…
Hi Drashti,
I understand that you are choosing R1 and R2 to configure the TLV1117 for 3.3 V and 5 V, but you mentioned you are not getting the desired output. What output voltages are you measuring instead?
Please also confirm that your load current…
Other Parts Discussed in Thread: TLV1117 Hi All,
I will going to use TLV1117 for 3.3V regulation and 5V regulation. I checked the datasheet and could not figure out the capacitor values.
I found some example circiut on web and they used ceramic caps…
Hi,
By voltage conversion time I assume you are referring to the startup time of these regulators.
1. The TLV1117 startup should be similar to the LM1117 shown in the following E2E thread. The time delay is slightly more than 0.5 ms.
https://e2e…
Hi Vishwajit,
TLV1117 is capable of 0.8 A output current. The current limit could activate at 1 A output current. If you need 1 A, you should choose another regulator rated for 1 A or higher.
The TLV1117-33 is a fixed 3.3 V output regulator, so…
Part Number: TLV1117 Hello Team
My custoner is using tlv1117ADJ. 12V->5V. The schematic is as follow.
and the output wave is as following:
If add more large value capitor, it will be ok. Is it
Part Number: TLV1117 Hello Team
My custoner is using tlv1117ADJ. 12V->5V. The schematic is as follow.
and the output wave is as following:
If add more large value capitor, it will be ok. if it have relationship with ESR? If yes, how to caculate…
Hi Bill,
Rja compared to Rjc will vary depending on the package. The DCY (SOT-223) and other similar packages like the DBV (SOT-23) can have very poor thermal characteristics and Rja > Rjc due to their small package size and lack of a thermal pad.…
Hi Alfred,
Unfortunately we do not have a model for this device presently. I suggest you to go for either of the following options.
1. You may either suggest your customer another compatible device whose model is available. For this, the following…