Part Number: TLV1117LV Hi,
We are planning to use TLV1117LV in our HMI tablet project. Our design requires 5 years of longevity. Please share the longevity/EOL details for the same.
Part Number: TLV1117LV Hi team,
My customer is using TLV1117LV to convert 5V to 3.3V. But there is a special use case in customer's design that the TLV1117LV input is not powered on but the output is connected to a 3.3V voltage. I want to check with…
Part Number: TLV1117LV Hi team,
There is no characteristic for foldback current limit vs Iout and temperature in the datasheet of TLV1117LV33, so could you provide the foldback current limit characteristic?
Regards,
Jun
Part Number: TLV1117LV Dear LDO experts,
The customer is evaluating our TLV1117LV. They want to know how the output accuracy changes with time. For example, what is the accuracy after it runs for one month or one year. So do we have the "Long-Term Stability…
Part Number: TLV1117LV Can you please verify the regulator package markings?
packaging said TLV1117LV12DCYR
We purchased these but the IC is marked as follows;
SI
35ZHC4H
Part Number: TLV1117LV Hi Team,
Sorry to bother you.
I would like to use TLV1117LV to support 4.5Vin/3.3Vout/1A application. Can this LDO support this condition?
Thanks a lot.
Yours Faithfully
Redick Lee
Part Number: TLV1117LV Hello Sir,
We are planning to use LDO TLV1117LV in our industrial project (working at high temperature grade).
Its junction temperature is up to 150 c(Abs max), our power dissipation (PD)= .586W.
Tj= (62.9*.586)+100=136.8, the junction…
Part Number: TLV1117LV Hello team,
Is there any risk if TLV1117LV works between the recommended maximum and absolute maximum input voltage?
The recommended maximum voltage is 5.5V, the absolute maximum voltage is 6V. However, in some condition, the input…