Part Number: TLV1702-Q1 Hi team,
My customer is using TLV1702-Q1. They want to know if 'Voltage Output Swing From rail' is the same spec like VOL?
And could we provide our test diagram/test circuit for this spec?
Regards
Michael
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: TLV1702
The Above Circuit is Designed to satisfy below requirement:
1. HIGH FOUT When LED Is Normal
2. LOW FOUT When LED is Fail Open
3. LOW FOUT When LED is Fail Short
4. LOW FOUT When VCC is…
Part Number: TLV1702 Other Parts Discussed in Thread: TLV7042 , TLV7032 , , TLV1704 , TLC3704 , TLV3704 Hello
We are considering to use TLV1720.
In our circuit, the output of TLV1720 must be high impedance.at low voltage below 2.0V.
Does TLV1720 behave like…
Part Number: TLV1702-Q1 Hi team,
When using only 1 channel out of 2 channels, how should I handle the unused 1 channel pins?
We are thinking the method that we will tie In+ to Vdd and In- tie to GND. The output terminal is open.
As we do not want to…
Part Number: TLV1702-Q1 Hi Team,
I have three question about TLV1702-Q1's output low level.
1. I Could you tell me the max Vol level?
2. Are there any equations to estimate Vol level at a temperature like 100C?
3. Could you tell me what "Voltage output…
Hello Alessandro,
As usual, Clemens is correct!
The model indeed does force the output to half supply when there is a violation of input range or supply voltage to alert the user that something is wrong...This is mentioned in the header of the model.…
Part Number: TLV1702 Hi,
Eastronics told me that the TLV1702AIDGKR is going to be announced as obsolete soon. The status shown in TI site is "Active".
Could you please check what's the TLV1702AIDGKR status? Can you please offer an alternatives…
Part Number: TLV1702-Q1 Other Parts Discussed in Thread: LMV7271 Hi,
Planning to use IC TLV1702-Q1 as a analog voltage comparator. Moreover, we have variable reference adjustment (i.e. from 0.5V to 10V & -0.5V to -10V ).
Question is, How shall I adjust…
Part Number: TLV1702 Other Parts Discussed in Thread: TLV1701 About TLV1702's output voltage swing, is there specification for temperature variation?
Datasheet is described 900mV (at Io ≦ 4mA), this spec is only 25℃ condition.
Best regards
Satos…