Part Number: TLV2186 Hi all
My customer is evaluating the TLV2186 in an application where the operating temperature of the device will go to max +45°C and they have this question:
Can you provide more detailed data on the input bias current up to…
Part Number: TLV2186 Hi,
I have a question regarding the max. output current of the op amp TLV2186. According to the datasheet, " Short-circuit to ground: continuous", it is safe to short the op amp output to ground.
But what about shorting the…
Part Number: TLV2186 I would like to use the TLV2186 to modify the feedback of a DC-DC converter, and I want to power the TLV2186 from the output of the DC-DC converter. During normal operation the output of the DC-DC converter ranges from 6 V to 10.5…
Part Number: TLV2186 I designed a sallen key topology 2nd filter by FilterPro.
then FilterPro shows me this conclusion
and there is no macro file in TINA TI.
so i downloaded tsm file and insert that( INSERT -> MACRO -> TLV2786.tsm)
and i designed…
Part Number: TLV2186 Other Parts Discussed in Thread: INA826 , OPA2196 , OPA2197 , OPA196 Hey there, I saw a circuit online to convert a 0-10V signal to 4-20mA current signal and I adapted it to 0-70V. The problem is that sometimes, when the circuit is connected…
Part Number: TLV2186
Hi,
Could you please tell me which value of the following "Figure 40" and "Table2" is correct regarding EMIRR IN+ ?
Best regards, Kato
Part Number: XTR116 Other Parts Discussed in Thread: TLV9052 , OPA391 , OPA187 , TLV2186 , OPA2187 , OPA2186 , OPA192 , XTR105 , OPA186 Are there any recommended circuit modifications we could make when using the XTR116U part that would allow the chip to go into…
Hi Jimbo,
I see that you like to use our full differential op amplifier, and we are very appreciative.
The Vref input requirement is a low impedance source, which means that it may be a voltage source that is capable to source and sink (Vref bandgap…
Hi Alvin,
The TLV2186 is a great low-cost part. It is a 24 V chopper with low power consumption, designed for sockets that need low-power, decent accuracy at low cost.
Otherwise also agree with Michael's suggestions above.
Best Regards, Mike
Hi Alvin,
OPA07C and TLV07 are very similar, but they come with a single die per op amp package. Both parts seem not in stock currently.
If you are looking for LM358, dual op amp package, the part seems to be available currently.
https://www.ti.com/product…