Part Number: TLV274 Other Parts Discussed in Thread: TINA-TI , TLV271 , TLV9154 Hi Team
My customer uses TLV274 as voltage follower.
My customer is referring the material (use TINA to confirm negative feedback stability, which is written in japanese) to…
Part Number: TLV274 Hi, Team
My customer wants to know if VOL will be less than 0.1V when IOH is about 3mA.
So my customer asked "what the worst values of VOH and VOL are when VDD= single 15V, TA=Full range, IOH=-1mA and 1mA respectively". …
Part Number: TLV274
Hello,
On my custom design PCB, I use multiple TLV274 type OpAmps for doing Howland Current pump configurations. Among eight of them, only two of the TLV274 is over heating. All of them is power with +5V and -4.2V. I checked all…
Raymond, thanks for the reply. I changed the op-amp to a TLV333 and the sensing now works great.
---------------------------------------------
I have a different design that uses a TLV274IPWR, that is buffering and filtering a 1200 Baud signal, and I…
Part Number: TLV274 Hi E2E experts ,
Could you please check for us if with a Single supply of 4.7V and GND the TLV274
can sink negative current from a current source connected to its outpur ?
Best regards ,
Arik.P
AFAE
Hello Yoo,
There are multiple sources of error besides initial input offset voltage. These include, but are not limited to, CMRR, PSRR, drift, shift, noise, and the error associated with the drift/shift of the device.
I highly recommend reviewing all…
Part Number: TLV274 Hello, In my design, I used an AOP TLV274 to rectify an AC signal. I meet this problem in some cases, the first amplifier of the package is destroyed. I don't understand why? A single supply of 14V is used to supply the amplifier…
Part Number: TLV274 Hi Team,
How is aged deterioration?Or aged deterioration included in the MAX value?
Input offset votage value (TYPE 0.5 mV, MAX 5 mV)
Best Regards,
Kenji
Part Number: TLV274-Q1 Dear Amplifier team
We have been serious problem which failed ES90000-2 spec in delamination for HKMC.
So, We search Zero delamination of TLV274QDRQ1.
Do you have zero delamination another item of TLV274QDRQ1 or Can you develop…