Part Number: TLV3201-Q1
Tool/software:
Hi team,
My customer is considering TLV3201-Q1, and from datasheet there is a note mentioned "Input signals that can swing more than 0.5V beyond the supply rails must be current limited to 10mA or less". Customer…
Part Number: TLV3201-Q1 Other Parts Discussed in Thread: TLV3201 , Hi,
In Auto driving solution circuit design,we need design a TLV3201 circuit for differential input which from the main connector
under 24V power input car system. Below is my design…
Part Number: TLV3201-Q1 Tool/software: Hi Team,
May I know how to judge whether our IC( TLV3201-Q1 ) can be washed?
After PCB assemble, manufacturing site might wash the PCB with pure water to clean the flux
I only receive this guideline from…
Part Number: TLV3201-Q1 Other Parts Discussed in Thread: TLV3201 , Tool/software: Why couldn't I confirm the 1kΩ resister of ESD protection stage from SPICE model of tlv3201.lib that described in Figure 26. TLV3201-Q1 Equivalent Input structure?
Why…
Part Number: TLV3201-Q1 Other Parts Discussed in Thread: TLV3201 Hello,
I have a question about Fig 25 from the TLV3201-Q1 datasheet. It seems the intent is to show that input voltages on either the IN+ or IN- pins of the device that exceed the rails…
Part Number: TLV3201-Q1 I am currently refereing to SNOAA40 Application Report.
If my Vcc=5V , And below is my requirement for current threashold.
DESCRIPTION
IG1 (A)
INA-OUT (V)-> [ Vref+(Amp Gain)(IG1*Shunt Value)]
VH, CHB
Overcurrent…
Part Number: TLV3201-Q1 Other Parts Discussed in Thread: TINA-TI , TLV3201 Hi Team,
Can you help explain how to calculate the VOH and VOL of this device at any temperature? Can you help me with these? Is there an application note that I can check? …
Part Number: TLV3201-Q1 Other Parts Discussed in Thread: TLV3201
Hi I have read the datasheet of TLV3201-Q1,
There has the curve of Output Voltage vs Output Current with full range temperature of 2.7V and 5.5V
but we are using 5V as the input voltage…
Part Number: TLV3201-Q1 Hi team,
I have a question about absolute maximum rating for TLV3201-Q1.
This device has both of voltage and current range for input pins. Is it no issue when the current at input pin is less than 10mA even if the voltage at…