Part Number: TLV320ADC3101-Q1
Dear TI experts,
Could you provide initial register settings(values) of TLV320ADC3101-Q1 for my customer?
I2C address : 0x18 (0001 1000)
MCLK : OSC 12MHz
Will test both AMIC and DMIC
I will attach the schematic…
Part Number: TLV320ADC3101-Q1 Hi Team,
Could you recommend a stereo ADC similar to the TLV320ADC3101-Q1? We require a higher SNR (greater than 92dB). Since it will be used for microphone inputs, built-in support for basic microphone input functionality…
Part Number: TLV320ADC3101-Q1 tlv320adc3xxx.c tlv320adc3xxx.h May I ask if this driver can be used? I found it in my SDK, I saw these commented out with if 0 in the official driver.
SND_SOC_DAPM_INPUT("IN_1L"),
SND_SOC_DAPM_INPUT("IN_1R"),
SND_SOC_DAPM_INPUT…
Part Number: TLV320ADC3101-Q1 Other Parts Discussed in Thread: TLV320ADC3101 Hi,
I would like to ask specifically about grounding and layout best practices for a low noise audio design.
System:
ADC: TLV320ADC3101 Q1
Microphone: IM73A135V01…
Part Number: TLV320ADC3101-Q1 tlv320adc3xxx.c tlv320adc3xxx.h Could you please help me with a reference and also provide some examples related to the device tree?
Part Number: TLV320ADC3101-Q1 Hi TI Team,
We are planning to use TLV320ADC3101-Q1 to interface our DMIC to the host processor.
The basic requirement we need from TLV320ADC3101-Q1 is a gain control support for the DMIC.
Can you please check and say…
Part Number: TLV320ADC3101-Q1 Hello,
Our customer used TLV320ADC3101-Q1 for his application, sampling rate is 32Kbps, Generating Master Clock from BCLK,
The captured data of ADC output which drew with MATLAB is not smooth as this:
Best regards…
Part Number: TLV320ADC3101-Q1
Hello,
Our customer used the TLV320ADC3101-Q1, input 200Hz 600mVpp sine signal, sampling rate is 16Khz.And captured the ADC
Max value: 10887
Min:-9460
Calculated the Vpp=1000*(10887-(-9460))/2/32768 = 310.4705811mV…
Part Number: TLV320ADC3101-Q1 "(R) SOB-413S42-FM H/F" Do you need to set up when using the microphone? Currently, the recording sounds very small when applied with this combination.