Part Number: TLV320ADC3101-Q1 Other Parts Discussed in Thread: TLV320ADC3101 Team,
I would like to know the sentence meaning of red rectangle.
And below is our measurement.
Is the result correct?
Roy
Thank you for your answer.
We are using TLV320ADC3101-Q1 for our circuit.
Which register of TLV320ADC3101-Q1 should I set the setting value that came out by pressing the "Coeff" button on the Biquad Coefficient Calculator?
Part Number: TLV320ADC3101-Q1 Hello,
i have a question to the mic inputs. In the datasheet there is a 1µF capacitor in parallel to the mic.
I think this is very strange because the capacitor shorts the Signal. Is the value correct?
thanks…
Part Number: TLV320ADC3101-Q1 I am confused by "Fig. 11 Typical Connections" from the TLV320ADC301-Q1 datasheet. Why are IN2R(P) and IN3R(M) connected to the same microphone? Same question obviously for the IN2L(P) and IN3L(M). I see that both IN2L and…
Part Number: TLV320ADC3101-Q1 Other Parts Discussed in Thread: TLV320ADC3101 Hi team,
I want to utilize digital microphone input of this device and setup using TLV320ADC3101EVM with digital microphone.
I sent BCLK(3.072MHz) to TLV320ADC3101 BCLK input…
Part Number: TLV320ADC3101-Q1 Other Parts Discussed in Thread: TLV320ADC3101 Hi team,
Could you give me the reference register setting for my use case below?
I am trying to connect digital mic to TLV320ADC3101 and output I2S at BCLK=3.072MHz.
Digital…
Part Number: TLV320ADC3101-Q1 Dear all, datasheet SLAS553B (rev. August 2015) reports at page 79:
In general, NADC must be as large as possible as long as the following condition can still be met:
MADC x AOSR/32 >= RC
RC is a function of the chosen…
Other Parts Discussed in Thread: TLV320ADC3101-Q1 , CC1350 Hello, I am considering doing a project on the wireless transmission of digital audio in the sub 1 GHz band. So the first step is to convert the analog audio into digital, and I see this codec…
Part Number: TLV320ADC3101-Q1 The ADC provides a “Dither control” register (Page 1, Register 26) but it is not described anywhere in the datasheet.
Could you provide some info about its intended usage? From the register description, it seems to work…
Part Number: TLV320ADC3101-Q1 Hello,
I was thinking of using the component TLV320ADC3101-Q1 to interface two digital (in PDM) and one analog microphones. I want to communicate with my CPU in TDM. In my application the digital and analog microphones…