Part Number: TLV320ADC5120 Hello, we have been using the TLV320ADC5120 for several years in one of our products and our application makes use of the internal biquads to create a custom high pass filter. We have never experienced an issue with register…
Part Number: TLV320ADC5120 Tool/software:
Hello TI Support Team,
We are currently working on TLV320ADC5120 IC. As part of our testing, we applied a 1 Hz sine wave signal with 200 mVpp to the ADC input. The ADC output waveform correctly shows a sinusoidal…
Part Number: TLV320ADC5120 Other Parts Discussed in Thread: PUREPATHCONSOLE I have requested to download the PUREPATHCONSOLE3 application over a day and a half ago. I still have not received approval for it.
Is there any way I can get this moving faster…
Part Number: TLV320ADC5120 Tool/software: Hello TI team,
Now I'm trying to enable the voice-activity-detection function(VAD) on TLV320ADC5120 EVK board, but failed: no interrupt occurs when the signal gets into EVK.
Here are some configurations: …
Part Number: TLV320ADC5120 Tool/software: Hello,dear expert: Our microphone project, one transmition and one receiver. The transmition use 5120, 5120 I2S output to telink. The receiver is telink UAC output. Now we encounter problem.It's when input small…
Part Number: TLV320ADC5120 Tool/software: Hi ti team,
1. At present, when testing 5mvRMS input, THD+N is below 0.2%, but the interference is relatively large when using the spectrum, as shown in picture 1 below.
Opening the DRE according to the chip…
Part Number: TLV320ADC5120 Tool/software: The data sheet states in Section 3, Description: "......allows for sample rates up to 768 kHz, and allows for sample rates up to 192 kHz." What is the sample rate of the sigma-delta AGC bock without upsampling…
Part Number: TLV320ADC5120 Tool/software: Hi TI Team,
In low power mode, We hope GPIO1 generates an interrupt signal to notify the host when a signal input is detected in channel 1 (differential input / PIN1&PIN2) or channel 2 (differential input /…
Part Number: TLV320ADC5120 Tool/software: I use TLV320ADC5120 to sample two types of data (four channels), one of which is an ECG chip "CN121". The ADC and MCU use I2S communication. My problem is that I2S can only call the callback function twice, and…