Part Number: TLV320ADC5140 The customer is using TLV320ADC5140 to sample four analog microphone signals.
Because the I2S host is a standard I2S and cannot be modified, only tlv320adc5140 can be connected to the standard I2S interface.
Whether it is…
Part Number: TLV320ADC5140 Other Parts Discussed in Thread: TLV320ADC6140 Tool/software: Hi here.
We are planing to use TLV320ADC5140 for our project. I'm fighting whit TVL320ADC5140 master + Raspberry Pi model 5 ---- 6.12.20+rpt-rpi-2712 in slave mode…
Part Number: TLV320ADC5140 Tool/software:
Hi,
We have two ADCs that are connected to a master. TI ADC MCLK is supplied by an external clock due to inaccurate samples received by the master when mclk is provided by the master. 4 channel inputs are…
Part Number: TLV320ADC5140 Hi Team,
The I2S on main control side only has one data, and need to send audio data exceeding 4 channels through TDM through two TLV320ADC5140 cascading.
Does this ADC support cascading of two TLV320ADC5140? Is there…
Part Number: TLV320ADC5140 Hi team,
Looking at the connection example described in the specification, the GND of ADC5140 is connected only to the AGND (the ▼ mark in the figure below).
DGND is connected to the DREG and IOVDD through a bypass capacitor…
Part Number: TLV320ADC5140 Hello!
As stated in the title, is the TLV320ADC5140 capable to convert a DC voltage? I see some mentions in the datasheet about DC coupling, but it's seems alto that an HPF is always applied to the input.
Thanks,
Marc…
Part Number: TLV320ADC5140
Hi, TI support team
My customer requested review for TLV320ADC5140 circuit.
- Customer name : MARUSYS
I will share more detail information of project and customer.
Since the material is confidential, I can share by…
Part Number: TLV320ADC5140 Hi
My customer care about data sampling time of TLV320ADC5140. So l would like to know what is t he delay time range of audio data from input pin to output pin?
Thanks.
Amber Si