Part Number: TLV320ADC6140
I’m the TI customer who originated this request :
https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1188564/tlv320adc6140-interface-nvidia-jetson-nano-to-tlv320adc6140
I’m currently not able to read acoustic…
Part Number: TLV320ADC6140 I am getting audio distortion when operating at 384kHz. I have turned off the DRE and AGC. I have also set the number of bi-quads to 0, but I cannot seem to get rid of the waveform distortion. At 192kHz and below, there is no…
Part Number: TLV320ADC6140 Hi Team,
We received this inquiry from our customer.
" We bought an acoustic board TLV320ADC6140 and we want to interface this board on a nvidia jetson nano. I understand that linux kernel can have a module to interface…
Part Number: TLV320ADC6140 Hi!
When connecting line-level (+/- 1.736V, 1.228Vrm) single-ended w/ AC coupling capacitors, is any external connection with MICBIAS needed? How are the INxP and INxM lines biased? There isn't much info on connecting single…
Part Number: TLV320ADC6140 Hi,
We're using the TLV320ADC6140 to sample signal from a microphone which it's lowest voltage level is -111dBV (5.6µV RMS ) . The mic connected differentially to the ADC.
The ADC is fed with 3V and VREF is set to…
Hi Prudhvi
According to datasheet TLV320ADC5140 Quad-Channel, 768-kHz, Burr-BrownTM Audio ADC datasheet (Rev. A) (ti.com)
TLV320ADC6140 Quad-Channel, 768-kHz, Burr-BrownTM Audio ADC datasheet (Rev. A) (ti.com)
Both chips can support
Multichannel high-performance…
Part Number: TLV320ADC6140 We have designed this part into a product, built it, and only now noticed the little comment buried in the data sheet mentioning an 80kHz bandwidth limit. Our application requires close to 100kHz audio bandwidth (2 channels…
Part Number: TLV320ADC6140 Sir,
I have interfaced ADC6140 with TI DSP C6747.
Configured ADC6140 for word len of 16 bits, single ended ac coupled input. PGA gain to 6 dB.
McAsp0 RFMT register at DSP is set to 0x00018078 // no rotation, 16 bits len, pad…
These settings are currently not provided to customers. The Automatic configrations are tested for functionality and reliability and are recomended. With manual settings you might encounter issues with certain timings. In order to avoid this we suggest…