Part Number: TLV320ADC6140 Other Parts Discussed in Thread: TPD2E2U06 , Hello guys,
Please tell me EAR number for below parts. TLV320ADC6140IRT LMR14030SQDPRRQ1 TPS62090QRGTRQ1 TPD2E2U06
If you have any questions, please don't hesitate to contact me. Best…
Part Number: TLV320ADC6140 Hello,
I know this forum dedicated to TI audio devices , but as Audio forum , I assume many people here familiar with Alsa buffer size.
From experiments we see that the maximal Alsa buffer is 32KB
When we trying to define…
Part Number: TLV320ADC6140 I need to connect a measurement microphone + preamplifier to a TLV320ADC6140 input.
The preamplifier is powered symmetrically with +5.5V and -5.5V so the signal is single ended and voltage vary in the range -5.5V/+5.5V which…
Part Number: TLV320ADC6140 we are using 2 devices of TLV320ADC6140 in order to sample 8 microphones simultaniosly
at the tha sheet its writen:
Ability to synchronize the multiple devices for the simultaneous sampling requirement across devices
could someone…
Part Number: TLV320ADC6140 Hello, I am trying to set the GAIN for each of the three channels I am using on the TLV320ADC6140 and I'm running into a problem. First a bit of general information: The TLV320ADC6140 is used in Audio Bus Master Mode, a microcontroller…
Part Number: TLV320ADC6140
my question is regarding ESD protection for input mic. ports of the TLV320ADC6140IRTWT
the microphons are connected throw 10 meter tweested pairs cable (diff mic.) and i have serial capacitor at the inputs
do i need esd protection…
Part Number: TLV320ADC6140
Hello,
In our project we connect 2 TLV320adc6140 (TDM , daisy chain) in order to get 8 input channels (Analog).
The CPU is the master ( provide FSYNC/BCLK and get back all samples in same RX line )
- I couldn't find in the…
Part Number: TLV320ADC6140
Hello,
I'm working under Linux(Debian) with 2 TLV320ADC6140.
Once the device driver loaded (by adding it to device tree) , both devices marked as UU (kernel use)
How should I access the I2C registers (read/write) from…
Part Number: TLV320ADC6140 Hi, I have the tlv320adc6140 working in a design and I now want to start using the biquad filters.
I installed PurePath 3 but I cannot find any reference to the tlv320adc6140. Is there a plugin that I am missing?
thanks.