Part Number: TLV320AIC1106 Hi,
TLV320AIC1106EVM-K not found on HP.
It would be very appreciated that tell me reason for Obsolete of TLV320AIC1106EVM-K.
Best Regards,
Nishie
Hi,
As mentioned in the comment above, the values are in hex where else the register address in datasheet is in decimal. They are the same register address.
Something in your system prevents the muting/unmuting.
Regards,
Peter
Part Number: TLV320AIC1106 Other Parts Discussed in Thread: TLV320AIC1110 Hello,
My customer is looking for an alternative device of AKM2306.
Their requirements are as follows.
compliant with ITU-T G.711
compliant with ITU-T G.712
u-Law codec
…
Part Number: TLV320AIC1106 Hello,
Q1:
Can EAROUT+ and EAROUT- drive differential 600 ohms load?
If yes, should the 600 ohms load be ac-coupled with EAROUT+ and EAROUT-?
And how much would the differential EAR AMP output voltage be when PCMI code is u…
Part Number: TLV320AIC1106 Hello,
I am using PCM output from this IC and for synchronization, we have to use PCMSYN. I am little confused that do we need to derive PCMSYN signal from Master clock of TLV320AIC1106 or we can connect the PCMSYN pin to micro…
Part Number: TLV320AIC1106 Hello,
I have designed a schematic diagram which includes the connection and input/output pins for TLV320AIC1106. I am using this IC to convert my input analog audio signal to PCM signal. But I am little confused that why are…
Part Number: TLV320AIC1106 Hello Sir / Ma'am,
Do we need any programmer to program TLV320AIC1106 & TLV320AIC1106EVM, if we to change its default programs.
Are this ICs pre-programmed or we have to program after purchasing them.
Thanks & Regards…
Part Number: TLV320AIC1106 Dear,
I cannot find TLV320AIC1106EVM, how to fine tune earout gain?
i just only see MIc Amp gain fine tune.
TLV320AIC1106EVM-K User's guide (Rev. A) (slau328a.pdf) http://www.ti.com/litv/pdf/slau328a
If any suggestion, Please…
Part Number: TLV320AIC1106 Other Parts Discussed in Thread: TLV320AIC3101
Dear,
our client design TLV320AIC1106 with MC8090( 3G Modle) was can work and sound was normal , but MC8090 was EOL.
so We change Air prime WP8548( 3G Modle) linear mode Audio sound…