Part Number: TLV320AIC1110 Hi team,
I am working with a customer who is looking for an audio CODEC solution that supports both of the following standards:
PCM CODEC Interface: ITU-T G.711 (u-law PCM)
ADPCM CODEC Interface: ITU-T G.726 (32kbps…
Part Number: TLV320AIC1110 Tool/software: Hi,
Please help me with the following questions:
I believe the analog signal applied to the MICxP/N pins of the TLV320AIC1110 is converted
to 16-bit two's complement digital data.
The ratio of the…
Part Number: TLV320AIC1110 Tool/software: Hi all,
I would like to ask about the frequency parameter of the voice through TLV320AIC1110.
For both boards mounting TLV320AIC1110, ・TX gain:29.5dB ・RX gain:-4dB setting, if you look at the frequency response…
Part Number: TLV320AIC1110 Tool/software: Hello, My customer has some questions for AIC1110.
1) The below is from the datasheet. Please see the yellow marked one. It says PCMCLK. But I think it is a typo and it should be PCMSYN. Is this understanding…
Part Number: TLV320AIC1110 Other Parts Discussed in Thread: TAC5111 Hi,
I'm working on verifying a custom board with TLV320AIC1110, but the loopback function isn't working as expected. So, could you please tell me the following?
Q1 Is it correct to…
Part Number: TLV320AIC1110 Tool/software: Hi team,
Should the VSS pin be connected to analog ground? The surrounding pins are digital pins and are not easy to handle. A recommended layout would be helpful, but since it doesn't seem to be available from…
Part Number: TLV320AIC1110 Tool/software: Hi team,
(i) Is 1.36 Vpp the maximum voltage level for EAR2? Overload-signal level (3 dB): There is also a value of 1.925V, I would like to know how I should consider this value. (For example, if 0dBm is increased…
Part Number: TLV320AIC1110 Tool/software: Hi team,
I would like to route the output of EAR2 to MIC1P,N and output on PCMOUT. However, due to the rule of input full scale voltage, I cannot use the output of EAR2 as it is, so I will input the output of…
Part Number: TLV320AIC1110 Hi,
I have a question about register settings for TLV320AIC1110.
■Question 1 <Power Control Register:00-1> This is a question regarding the timing of powering on the Reference System and canceling the power down of the channel…
Part Number: TLV320AIC1110 Other Parts Discussed in Thread: TLV320AIC1103 Hi,
I have two questions about the power supply of the TLV320AIC1110.
Q1. Is it OK as long as VDD adheres to the rated 2.7V~3.3V? In other words, does VDD need to be 3.0 V?…