Part Number: TLV320AIC14K Tool/software: am using one TLV320AIC14K in my circuit as a stand alone slave, can i use an external crystal oscillator to generate 20mhz clock for the MCLK of the TLV320AIC14K, and then use the microcontroller to generate my…
Part Number: TLV320AIC14K Other Parts Discussed in Thread: TLV320AIC3100
Dear Team, hello, I am reviewing the TLV320AIC3100 product for the purpose of replacing the audio chip I was using.
The circuit is already written, and I must have to replace…
Part Number: TLV320AIC14K Hi ...
We are using TLV320AIC14KIDBTR in one of our audio processing card.
The input to the TLV320AIC14KIDBTR will be MICIN or 1.5 Vrms differential signal.
The output of the TLV320AIC14KIDBTR will be given as an input…
Part Number: TLV320AIC14K Holle E2E,
Our customer is testing the new board that it using the TLV320AIC14K. At airborne noise, the device has latched up and stop, it has heat. After, the device make reset operation from MCU, but the device has heat still…
Part Number: TLV320AIC14K Other Parts Discussed in Thread: TLV320AIC3107 , TLV320AIC3100 Hi team,
The customer would like to select a audio codec. His requirements are as below:
Input: Analog audio source
Output: Class D audio amplifier
The codec…
Part Number: TLV320AIC14K Other Parts Discussed in Thread: TLV320AIC3262 , TLV320AIC3268 Please let me know about specification for TLV320AIC14K below.
①Max output power in the case of 6Ω Headphone/Speaker.
②Is TLV320AIC14K have below function?
…
Hi, Jorge,
The TLV320AIC14K data format is 2's complement signed. This is the data format in the most part of our codec devices.
Best regards,
Luis Fernando Rodríguez S.
Other Parts Discussed in Thread: TLV320AIC14K Hello,
I've read through the datasheet and have a question about programming this device.
It says in the Host Port Interface section on pg 27 that this I2C interface can be used to program the devices…
Other Parts Discussed in Thread: TLV320AIC14K Hello,
I see on TLV320AIC14K datasheet that gain of the "INP and INM Input" can be adjusted from -42dB to 20dB in 1dB steps.
I wonder if this gain setting refers to voltage or power. My question is, in…