Part Number: TLV320AIC23B Dears:
May I consult you one thing regarding TLV320AIC23B audio codec’s THD under AVDD=2.7V for Analog Linein to Lineout, bypass mode?
In bypass mode, analog linein to analog lineout, AVDD=2.7V, test conditions are shown…
Part Number: TLV320AIC23 Hello,
I am looking for TMS320VC5509A DSK BOM (Bill Of Materials) to find the 3.5 mm jacks' part numbers and their footprints.
In my designs, I always use 5-pin 3. mm jacks like the images below:
In addition, related to…
Part Number: TLV320AIC23 Dear all,
I'm working with TMS320C6713 DSK. What is the maximum Peak to peak sinusoidal voltage can be applied at line input of Audio codec TLV320AIC23
Part Number: TLV320AIC23 Hi,
I have problems to configure a TLV320AIC23BP to output stereo output to a headphone. I get just high frequent beeping.
The TLV320AIC23BP is connected as slave to a STM32 using the „MSB first, left aligned“ format, full duplex…
Part Number: TLV320AIC23 During my research for my project I decide to choose TLV320AIC23 as my audio codec. I search for a evaluation board and found TLV320AIC23EVM2 but TI stop the production and I would like to know why ?
Part Number: AM6548 Other Parts Discussed in Thread: AM6528 ,
We use am6528 + tlv320aic23, now it can work in I2S mode, but only left channel output sound normally, there is no output with RHPOUT, we measure the signal of FS and AXR0 with oscilloscope…
Part Number: AM3359 Other Parts Discussed in Thread: TLV320AIC3104
Team,
Can you please assist with the question below from my customer?:
I am really struggling with an issue of connectivity between the AM3359 and a TLV320AIC23B CODEC using the pinmux…
Part Number: TLV320AIC23 Hi All - I wondered if anyone knows if the TLV320AIC23 part can perform sample rates below 8kHz by applying a suitable input MCLK and divider? I'm looking to perform a custom sampling at 7.111kHz. Any guidance on best clock…
Part Number: TLV320AIC23 There are LLINEIN/LOUT and RLINEIN/ROUT as the stereo feature of TLV320AIC23.
Can I use them as two independent input/output channel ?
That is, one mono channel is LLINEIN/LOUT, and another independent mono channel is RLINEIN…