Part Number: TLV320AIC23B Tool/software: WEBENCH® Design Tools Hi all,
Using the TLV320AIC23EVM2 for configuring the register by SPI,and GUI use our own SPI tool.Now i want to know if my connection is right.
In master mode :
My connection is following…
Part Number: TLV320AIC23B Hi all,
I have a problem about register REG LRS/RLS Left/right line simultaneous volume/mute update for Left/right line input channel volume control (Address: 0000000 Address: 00000001).
1、 First,I choose the LRS bit, then i…
I am reading 7.3.11 Clock Generation and PLL and
7.3.12 Digital Audio and Control Interface
I am finding it hard to understand all the details and interactions.
Given the existing I2S clocks generated by my DSP and the fact that they work properly with…
Part Number: TLV320AIC23B Hello,
I am trying to use the TLV320AIC23BIPWR Codec with a dynamic microphone and a piano amplifier. For the input to the ADC, I figured an anti-aliasing filter couldn't hurt the signal processing in the Codec.
However, I…
Part Number: TLV320AIC23B Topic: Audio CODEC, regarding TLV320AIC23B’s Analog-line-input-2-line-output bypass mode THD under AVDD=2.7V
TI FAE:
Sir/Madam:
May I consult you one thing regarding TLV320AIC23B audio codec’s THD under AVDD=2.7V for Analog…
Part Number: TLV320AIC23B Tool/software: Code Composer Studio dear :
is TLV320AIC23B can configure the data format for mono playback and recording? because the input data is mono. Thanks
Part Number: TLV320AIC23B Hi Team, Currently helping our customer on debugging issues with their TLV320AIC23B board. Is it allowed to configure the codec (by SPI) and in the same time transmitting and receiving data from the McBSP channels? Kind Regards, …
Part Number: TLV320AIC23B In my design, I have AVDD=BVDD=3.3V and DVDD=1.8V
What will be the logic levels for I2S signals?
And similarly what should be the oscillator supply voltage in case if I use external clock on XTI/MCLK?
I believe both of these…
Part Number: TLV320AIC23B Dear expert,
I use AIC23B to play and record audio, aic23b works as Slave, MCU as Master, I2S mode. MCU provide LRCIN and BCLK. play sound is good, but recording sound is very not clear with periodicity noise.
the AIC23B init…