Part Number: TLV320AIC3007 Tool/software: Hi all,
We designed the schematic using the TLV320AIC3007, but in a design refinement it doesn't output audio anymore .
Here's the altered schematic, where SAI5 is a 1.8V level signal.
Here's the schematic…
Part Number: TLV320AIC3007 Tool/software: I have observed that when i.e. the LEFT DAC is playing a tone, it is coupling to the path of the RIGHT DAC when the RIGHT path is connected (or any other path than DAC L1) to one of the output with an attenuation…
Part Number: TLV320AIC3007 Tool/software: Hi,
we intend to make a Yocto image for our IMX8 carrier board. The linux kernel is 6.1.6 and we are using the existing TLV320AIC3x driver (
* ALSA SoC TLV320AIC3x codec driver I2C interface * * Author: Arun…
Part Number: TLV320AIC3007 Hello,
Our customer is in feasibility study phase to employ TLV320AIC3007.
Here is curiosity of signal separation performance between MIC1L to MIC2L or MIC3L.
The datasheet is specified between MICxL to MICxR performance…
Part Number: TLV320AIC3007 Is Above codec supports full-duplex communication ?Let us Say, There are two systems each with 1 codec acting 1 as transmitter and another receiving. Is it possible to speak in mic and hear at speaker data coming from another…
Part Number: TLV320AIC3007 Other Parts Discussed in Thread: TLV320AIC3107 Hello,
I have a question about TLV320AIC3007 Power Supply Sequencing. I couldn't find the Power Supply Sequence data in the TLV320AIC3007 datasheet. Is it the same as Figure 37…
Part Number: TLV320AIC3007 Hello team,
Can you tell me the overall current consumption of TLV320AIC3007 with following condition?
- DVDD: 1.8V±3%
- Other power supplies: 3.3V(Min:3.234V、Max:3.366V)
*Speaker is also driven by 3.3V power supply…
Part Number: TLV320AIC3007 Hello,
Our customer is evaluating TLV320AIC3007 ADC noise include analog PGA function.
We have two concern, first one is "noise floor vs PGA gain" is changed not linear response.
Attached waveform is noise floor level…
Part Number: TLV320AIC3007 Hello,
I would like to set fade-in / fade-out on the TLV320AIC3007.
Could you tell me how to set the registers and timing?
Best regards, Nomu