Part Number: TLV320AIC3007 Other Parts Discussed in Thread: TLV320AIC3104 , , TLV320AIC3107 Hi Team,
I'm trying to understand the key differences between the TLV320AIC3007 vs the TLV320AIC3104 and why the '3007 is priced higher than the '3104.
Thanks…
Part Number: TLV320AIC3007 Other Parts Discussed in Thread: TLV320AIC3100 Dear TI-Community,
according to the TLV320AIC3007 datasheet the "mono class-D output is capable of differentially driving an 8-Ω speaker.". Other Codecs of the TLV320AIC3XXX-family…
Part Number: TLV320AIC3007 Tool/software: Linux We are checking the availability of commercial version of Linux device driver for Audio Codec - TLV320AIC3007.
We have to interface TLV320AIC3007 to Yocto Linux (kernel version 4.12) image for IMX6UL.…
Part Number: TLV320AIC3007 Hello TI Team,
I've a feedback from the SW team regarding the TLV320AIC3007 chip.
In fact when we switch on and off the board (so the IC), there is a plop sound in the Class D output (pin19 and 20).
Schematic is the…
Part Number: TLV320AIC3007
Hello Anybody,
I have board based SoC realtek and codec TLV320AIC3007IRSBR which connected via I2S bus to SoC. 3 microphones are connected to codec - LINE2LP+LINE2LM, LINE1LP+LINE1LM, LINE1RM+LINE1RM and all are configured…
Part Number: TLV320AIC3007 Hi,
When i am playing audio with aplay command blank screen is coming its not terminating it self until given ctrl+c.Please have a look on dump data of codec and log.
Please have a look on below log.
We got below dump…
Part Number: TLV320AIC3007 Hi
Im using the TLV320aaic3007 codec for my project , facing problem with the mic recording when i record something with the pre recorded with volume high mic records it and can be heard on the speaker,but when i record my…
Part Number: TLV320AIC3007
HI,
I am interfacing tlv320aic3007 codec on my carrier board,here codec working as slave mode.In slave mode audio is not working but if i use in master mode audio is working.Please have a look on below details.
1)when…
Hello,
We'll need more information about what's going on to help resolve this. Have you selected and powered-up the ADC channels with the desired input configurations? Until then there's a lot of good information already available on this forum about…