Part Number: TLV320AIC3104-Q1 Hello,
For one of our projects we've verified this routing on your side, we had to feed left_lop/m feedback to mic input as on the attached image, this configuration will not be used in another variant so is it okay to…
Part Number: TLV320AIC3104 Tool/software: Hello, Does TLV320AIC3104 produce its own internal MCLK if BCLK is supplied by the host processor. Its mentioned in the datasheet (fig below).so if MCLK signal is absent from host processor, is BLCK is just enough…
Part Number: TLV320AIC3104-Q1 Questions about the TLV320AIC3104-Q1
1.Can we consider 6PAIC3104IRHBRQ1 and TLV320AIC3104-Q1 to be the same device?
2.Please review our schematic. A cable goes to an external microphone; the audio signal comes in from…
Part Number: TLV320AIC3104 This is a continuatio of previous questions I had which was incorrectly marked as "RESOLVED"
I have a TLV320AIC3104 Dev Kit. It is connected to a ESP32 S3. I have set the I2S intface such that
wclk = 16KHz, bclk=512KHz,…
Part Number: TLV320AIC3104 Other Parts Discussed in Thread: OPA1622 , Tool/software: Hello team ,
I've used OPA1622 to drive my 10 ohms receiver and it is working fine . I have 2 major concerns now:
For audio applications i have to use single or dual…
Part Number: TLV320AIC3104 Other Parts Discussed in Thread: TAC5212 Tool/software: Hello team ,
Can i increase my codec TLV320AIC3104 dynamic range by " range switching in DAC" ?( I'm using Headphone outputs )
If not ,
How can i increase dynamic…
Part Number: TLV320AIC3104 Other Parts Discussed in Thread: OPA1622 Tool/software: Hello team ,
Can i use TLV320AIC3104 codec with receiver DD45 (headphone output ) .
My codec output impedance is 16 ohm and this receiver has 10 ohm o/p impedance …
Part Number: TLV320AIC3104 Tool/software: Hi Team,
I’m using the TLV320AIC3104 codec and I see that the dynamic range of the stereo headphone output is around 91 dB as per the datasheet. I need to increase this dynamic range — ideally up to 120–130…
Part Number: TLV320AIC3104 Other Parts Discussed in Thread: TAC5212 Tool/software: Hi Team,
I’m working on an audio project using codec TLV320AIC3104 . I need to increase the dynamic range of the codec.
What are the recommended ways to achieve…
Part Number: TLV320AIC3104 Tool/software: Hi Team,
In the EVM board of TLV320AIC3104 EVM, the motherboard is AC-MODEVM which has XMOS IC on it. I want to use only daughter board of EVM as I'm using external MCU (nRF5340/nRF52832 DK) for I2C and I2S…