Part Number: TLV320AIC3104-Q1 hi,
Play music in the background first, then run the recording, in & out at the same time as the music that will be recorded to the playback!
How to solve this problem?
Here is register dump while recording:
[ 0]--00…
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: TLV320AIC3104 hi
The circuit diagram is attached, what if the current circuit to improve the MIC noise problem?
Are there any recommended values for C838 and C839?
The problem is that the recording…
Part Number: TLV320AIC3104-Q1 Hi,
A customer is developing a product using the TLV320AIC3104-Q1.
We ask if it is possible to set the HP OUT level to 1Vrms or more.
[Input Condition]
0dB input Full Scale
How much Vrms output comes out when 9dB is set…
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: TLV320AIC3104 ,
Hi,
Regarding TLV320AIC3104,
our requirement from the audio codec are:
1.) 1x Audio Input: differential
2.) Analog Input voltage swing 1Vp-p of differential input:
does the…
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: TLV320AIC3109-Q1 , , TLV320AIC3254-Q1 , TLV320AIC3104 Hi TI-team
My customer want to know about TLV320AIC3104-Q1 and TLV320AIC3109-Q1.
These data sheets have a Codec.
Do these ICs have the function…
Part Number: TLV320AIC3104-Q1 Hello Landon,
Good day.
Our customer would like to know, if by muting the left PGA, can he put the LINE1LP input impedance into an extremely high state?
Refer to the image below.
Thanks in advance!
Art
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: LM48310 , , TPA2000D1-Q1 , TPA2005D1-Q1 hi
I have two questions:
1. "tlv320aic3104-q1 + lm48310+2W/4ohm SPK" Is this combination right? Is there any other AMP recommended? My demand is MONO …
Part Number: TLV320AIC3104-Q1 Hi team,
could you help review TLV320AIC3104-Q1 schematic? customer application is 1-ch MIC input , 1-ch audio output.
and, I alos would like to know what's the maxmium operate power consumption during full operating temepratue…
Part Number: TLV320AIC3104-Q1 Hi Aaron ( Aaron Estrada51 ),
Regarding my questions about TLV320AIC3104 ,
The spec for our audio input line was updated to 2Vrms voltage input level .
also, we still need to stand for the next requirement:
1.) 1x Audio Inpu…
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: TLV320AIC3104 Hi Team,
My customer now use TLV320AIC3104 in their project. And found some issue.
There will be a pop sound when the call is first connected, and there will be this pop sound…