Part Number: TLV320AIC3110 Other Parts Discussed in Thread: TLV320AIC3206
I am building an aviation headset in the medium term but am currently building a test board to try a few things out first. I am making use of a single speaker, stereo headphones…
Part Number: TLV320AIC3109-Q1 Other Parts Discussed in Thread: TDA4VM , TLV320AIC33 , TLV320AIC3007 , TLV320AIC3106 , TLV320AIC3104 , TLV320AIC3100 , TLV320AIC3110 , TLV320AIC3120 , TLV320AIC3111 , TLV320DAC3100 , TLV320DAC3101
Hi,TI
Now we are debugging tlv320aic3109…
Part Number: TLV320AIC3110 It is mentioned in section 7.3.11.1 of the datasheet, that lower power can be achieved by deriving clocks from simple dividers, and NOT using the PLL. I can't find anywhere, how much power that would be expected to save (i.e…
Part Number: TLV320AIC3110 From the specification, we have Tj(max)=105℃ and Ta=85℃, Rθja=32.7℃/W, Rθja=23.3℃/W
Can we use Tj = Ta+ Θja * P to calculate the power consumption? Is Ta=85℃ when Tj(max) is 105℃?
In other words, which formula…
Part Number: TLV320AIC3110 Hello. TLV320AIC3110 has a lot of settings and I'm confused. Also, SAI in STM32 has much more settings than just I2S, I don’t understand how to make these two things work together.
I do not understand what to specify…
Part Number: TLV320AIC3110 Hi,
I'm new to using the TLV320AIC3110 and have been trying to get basic headphone operation working using the Example Register Setup to Play Digital Data Through DAC and Headphone/Speaker Outputs documented in section 7.3…
Part Number: TLV320AIC3110 We are debugging Audio IC TLV320AIC3110 sent by FPGA signal to TI. The sound output will be truncated if the signal is higher than about 2.3v, resulting in noise in the sound output. If the volume input is small, there will…
Part Number: TLV320AIC3110 Dear Sir,
We checked AIC3110 DRC have some questions need your help,
Register:
Page0 REG68 0x44( DRC Control 1)
Enable
Page1 REG38 0x26 (Left Analog Vol to SPL)
91
Page1 REG42 0x2A (SPL Driver)
0C
Page0 REG65 0x4…
Part Number: TLV320AIC3110
Hi,
If PLL P/R/J register value is changed while device working, does PLL frequency vary immediately?
(I'm recognizing that its control is not recommended.)
Best Regards,
Kuramochi