Part Number: TLV320AIC3204 tHello team,
My customer is only using ADC for this device. (No DAC)
They are observing DC offset drift of +/- 5mV for the ADC, and they are struggling to calibrate this offset, because it drift with time/temp.
They are calibrating…
Part Number: TLV320AIC3204 Hi *,
this question has been asked before, but the previous thread (see here ) was closed without offering a solution. We are using a design identical to the Audiosense Pi Hat for the Raspberry Pi (same schematic, just a different…
Part Number: TLV320AIC3204 Hi, The AIC3204 specifies input channel separation with the following test conditions. 1kHz sine wave input at -3dBFS Single-ended configuration IN1_L routed to Left ADC IN1_R routed to Right ADC, Rin = 20kΩ AGC = OFF, AOSR…
Looking at your registers above; see attached with my comment, I noticed the following:
Your clock settings are for 22.1KHz fs and PLL is disabled.
Your HP power is from AVDD, but AVDD LDO is powered down.
8863.register.txt
PAGE0:
0 1…
Part Number: TLV320AIC3204
② #B to #A is normal.
① The voice received by Din(I2S 24bit) passes through the DAC and is not heard from the HPL. Is there anything I set wrong in the register below?
The register below is the register of #A. The register of…
Part Number: TLV320AIC3204 Hello
Is 8KHz the minimum configurable sampling frequency for TLV320AIC3204? 4kHz and 2kHz can be set, but are they not supported?
Thanks,
Takenari
Part Number: TLV320AIC3204 Other Parts Discussed in Thread: TLV320ADC3101 , TLV320AIC3101
Hi Team,
My customer is using TLV320AIC3204 and connecting the IN1_R、IN1_L as shown in the following diagram, and have noticed random DC offset at the output.
They've…
Part Number: TLV320AIC3204 Hi:
We encountered a problem .
A product with 8531+3204, which 8531 provides mclk, bclk, lrclk. When I lightly tap the device with my hand, the uplink and downlink data of 3204 disappear. The device must be restarted to…
Part Number: TLV320AIC3204 Hi,
I want to tie a TDK/Invensense ICS-43434 MEMS microphone to a TLV320AIC3204 CODEC.
At the moment, I am providing the MEMS with a 1.024MHz BCLK and a 16kHz WCLK. In return, I the MEMS outputs an I2S signed 24-bit 16kHz MSB…
Part Number: TLV320AIC3204
Hi Sir,
My customer is design AIC3204 but their host can't read AIC3204's I2C address (0x30). Does AIC3204 need clock (MCLK or...) as reference clock to process I2C communication? Or any point we have to check if AIC3204 is…