Part Number: TLV320AIC3204EVM-K Tool/software: Linux Hi all,
I try to communicate with Beaglebone Black via I2C2 bus, like below:
+ SCL(P12_16) -> P9_19 on BBB
+ SDA(P12_20) -> P9_20 on BBB
The position of SW1 is "I2C" and SW2 is "LOW". Although…
Part Number: TLV320AIC3204EVM-K Hi Sirs, Would you pls advise how to setup the AIC3204 EVM and its driver in Windows 10? Thank you and Best regards, Wayne Chen 08/25/2017
Part Number: TLV320AIC3204EVM-K Other Parts Discussed in Thread: TMS320C5535 Tool/software: Code Composer Studio Hello,
Finally I got it. 192 kHz of sample rate using filter B and with a BIQUAD filter to compensate the signal attenuation of 24 dB (4dB…
Other Parts Discussed in Thread: TLV320AIC3204EVM-K Hi,
I'm using the adapting filtering tool from the TLV320AIC3204EVM-K to make a bandpass filter. I already "recorded" the script for the real time coefficients, the ADC and DAC, and executed the command…
Part Number: TLV320AIC3204EVM-K I am attempting to set up an audio IP on IP1 and send it to line out via the digital loopback path. If I use the analog capability to do the same thing, everything is OK. It appears the problem is in the ADC/DAC, perhaps…
Part Number: TLV320AIC3204EVM-K Hi ,
There's one issue when I use TLV320AIC3204EVM-K.
Software :AIC3204 CS
Procedure( TLV320AIC3204EVM-K connected to PC via USB,and run AIC3204 CS)
1, Audio recording :choosing Differential on board microphone…
Other Parts Discussed in Thread: TLV320AIC3204EVM-K , TLV320AIC3204 Hi all, My customer has questions about TLV320AIC3204EVM-k GUI. 1. TLV320AIC3204EVM-K can operate up to 48ksps due to the speed limitation of TAS1020. Is it correct?
2. When customer…
Part Number: TLV320AIC3204EVM-K Other Parts Discussed in Thread: TLV320AIC3204 Hello,
I have a working TLV320AIC3204 PCB and I have been controlling the DSP settings with the MCU.
but I want to setup the whole configuration using EVM GUI first and…
Part Number: TLV320AIC3204EVM-K Other Parts Discussed in Thread: TLV320AIC3204 Tool/software: Linux Hello Team,
My customer are trying to activate the evaluation board in standalone mode vis-a-vis with the NVidia Jetson TX2 (The Jetson is running…
Part Number: TLV320AIC3204EVM-K Other Parts Discussed in Thread: TLV320AIC3204 Hello TI.
This is Jonathan form Avnet Korea.
One of our customers is developing audio system by using the TLV320AIC3204 & EVB, and the customer verified audio output by…