Part Number: TLV320AIC3206 Page 0 / Register 4 / bit D6 allows you to set the PLL range
0: Low PLL Clock Range 1: High PLL Clock Range
When should this bit be set to 1 instead of 0?
Part Number: TLV320AIC3206 Hello,
I'm bringing up a board with the tlv320aic3206 and having issues with the Ref pin. I followed example 4.3 from SLAA463B with a common mode voltage setting of 0.9V. I don't see the voltage at the Ref pin go above 0V…
Part Number: TLV320AIC3206 Hello,
I have programmed the CODEC using example setup 4.2 from slaa463b. I can measure a 1kHz sine wave at the analog input and can route the analog signal in the CODEC to the line out and headphone out and hear the sine wave…
Part Number: TLV320AIC3206 Hello Expert,
I need your help for schematic review and want to send schematic by private e-mail.
Here is my email : michael.jeong@arrow.com
If you send a email to me and then I will send it to you.
Also, when I check Linux…
Hi Nakano,
By default there will be no connections made so some settings will have to be written. But you can use the analog bypass path, and with 0 gain applied you should get something close to the same input you put in.
Best regards,
Jeff
Part Number: TLV320AIC3206 Dear forum members,
I am using a TLV320AIC3206. While playback works flawlessly, the microphone volume is currently way too quiet to be usable. The quality seems fine. I was wondering whether my setup might be wrong or if there…
Part Number: TLV320AIC3206 Hi, the Bluetooth receiver we're using (CSR8675) does not output MCLK. From the app note, the internal ADC and DAC clocks can be derived from BCLK, WCLK as well. Is MCLK absolutely needed for device operation? If yes, does TI…
Part Number: TLV320AIC3206 Hello,
The datasheet lists the ref voltage as 0.9V typical, but there are no min/max. Do we have any data on the min/max value? My customer is seeing 945mV
Thanks,
Michael
Part Number: TLV320AIC3206 Hello,
My customer is trying to put the device in shutdown mode. If all the supplies are present, but reset is pulled low, it consumes quite a bit more power than the 10uA listed in the datasheet. Is there more required to shutdown…