Hi Caleb,
Driver only set the samplerate register, it won't do any resampling. Kernel mainly focus on controlling instead of data processing. If you set the register samplerate to 44.1kHz, all of the audio data must be resampling to 44.1kHz before…
Part Number: TLV320AIC3254 We’re trying to get a TLV320AIC3254 codec running on a pair of custom boards. Both boards have a CC2652RSIPMOTR that are acting as masters and generating the clock lines and are using the SimpleLink Audio Plugin (v3.30.0.06…
Part Number: TLV320AIC3254 Other Parts Discussed in Thread: TLV320AIC3204 Hi Team, Due to procurement challenges our customer is considering to use the TLV320AIC3254 in lieu for their TLV320AIC3204 design. Apparently the only difference them is the embedded…
Part Number: TLV320AIC3254
Hi, Support Team
TLV320AIC3254 colud support 44.1khz/16bit or 44.1khz/24bit sampling rate?
if yes, Please share document for us to reference and how to program?
Thank you
Best regards,
Lawrence
Hi,
PLL review comments:
Page 0, R4 : PLL_CLK is input to CODEC_CLKIN, but there is no source selected for for PLL_CLK [D3:D2]
PLL Settings are; P=1, R=1, J=4, D=0
NDAC=1,MDAC=8,NADC=1,MADC=48,DOSR=192,AOSR=64. Is below expected settings?
Please us…
i will explain myself again maybe there is a mis communication right now im looking at the Analog input to I2S digital output side only. ADC side. im providing MCLK= 12.88MHz to the TLV30AIC3254. the input is audio jack (line/mic). the output is going to Header…
Part Number: TLV320AIC3254 Hi Sir,
My customers need the AEC, ANR, and EQ functions for the audio codec.
The application is used for DashCam.
May I know if the TLV320AIC3254 is a suitable device? or could you please advise which one is suitable?