Part Number: TLV320AIC3268 Hi teams
I have some question about tlv320aic3268. My customer use tlv320aic3268 with no AD/DA ,it works well. But when he configure the AD/DA and run them, Nothing output for the PN. the configure code as
follow,Could you…
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: PUREPATHSTUDIO Hello
We are developing a wearable audio product that requires multi-channel digital mixing and some light signal processing.
As a part of this system we need an audio processor…
Part Number: TLV320AIC3268
Dear Sir,
My application of TLV320AIC3268 is simple, 3 channel I2S in/out , 1 LINE out and 1 phone out to amplifier. The Speaker, REC,MIC are unused in my application. Because of unused function, how these power pin ( SVDD…
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: TPA3132D2 Dear sir,
In my application needs two line out (analog output), one is to connector directly, another is connected to class-D amplifier (TPA3132D2). But the TLV320AIC3268 has only…
Part Number: TLV320AIC3268 Hi Sirs, We got headphones distortion with CodecControl's example configuration. With 48kHz and 44.1kHz I2S, there are 2nd and 3rd harmonics with 1kHz test tone playback, and complete distorted signal with 10kHz test tone. Would…
Part Number: TLV320AIC3268 Hi,
I am using AIC3268 miniDSP to create a stereo multiplexer component for mux select.
There are 3 stereo channel inputs and one stereo channel output in the mux.
The below is mux properties in the PurePath Studio GDE:
Component…
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: PCM1864 Tool/software: TI-RTOS
TLV320AIC3268
Can I collect 8 channels of different audio at the same time?
Part Number: TLV320AIC3268 Hello,
Input impedance of analog inputs is 10K/20K/40K according the RIN setting in registers.
But I'm not quite understand what's the device input impedance if I put R1/R2 in the circuit as below:
Should the device…
Part Number: TLV320AIC3268 Hi,
I am using the AIC3268 codec on our custom board and use PurePath™ Studio GDE to program miniDSP.
I have successfully created header file from miniDSP program and write all register value that from header file to AIC3268…