Part Number: TLV320AIC3268 Could you please review the attached schematic for errors, suggestions, or criticisms?
TLV320AIC3268IRGCT Schematic Review.pdf
We are a small company, and board spins are expensive!
I appreciate any and all input.
Thank you…
Part Number: TLV320AIC3268 Hi Team,
We have plans to replace the ADI ADAU1451, but not sure if it is compatible with ADI's Sigma Studio, how do we transfer to the AIC3268?
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: TLV320AIC3262 Hi Team
Noticed AIC3268 has 3 lanes I2S interface. do they can work simultaneously with different clock sample rate?
if not, is there any other device can meet this requirement? …
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: AM3352 Hardware: AM3352 connected to codec TLV320AIC3268 via I2C and I2S
I am controlling the codec using I2C directly from a user-space application.
Can I produce sound over I2S bus without…
Part Number: TLV320AIC3268 Currently, I have the HPL and HPR signals going directly to a stereo jack.
What is the proper way to protect these outputs from ESD when someone plugs in a headphone without affecting the output?
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: PCM1808 ,
Hello folks,
I am trying to connect a PCM1808 with ASI3 of the TLV320AIC3268 using I2S, but I do not have signal on the headphone output. For the tests I did a simple connection, please…
Part Number: TLV320AIC3268 Dear Team,
I'm using TLV320AIC3268 Codec in my custom module.
To validate the audio performance, I need to generate side tone from Codec.
Kindly share the procedure to generate side tone (3dB down from actual audio signal…
Part Number: TLV320AIC3268 I did a firmware design several years ago for a client who was using the TLV320AIC3268 with an external AK4558 32bit CODEC. The AK4558 is not currently available, due to a fire in the production facility. My client originally chose…
Part Number: TLV320AIC3268 Guys,
I am using a pot to adjust to adjust the volume control on the headphone.
The headphone output volume control varies from -6dB to +14dB (B0_P1_R31 and B0_P1_R32).
Is there a nice way to ramp the audio levels from the previous…