Part Number: TLV320AIC3206 Hello Expert,
I need your help for schematic review and want to send schematic by private e-mail.
Here is my email : michael.jeong@arrow.com
If you send a email to me and then I will send it to you.
Also, when I check…
Part Number: TLV320AIC3206
Greetings,
I have a customer looking into using the TLV320AIC3206.
The customer has the following question:
Is a special driver required for use of this IC?
I am assuming I should refer them to the following…
Hi,
We have many devices that can support 3.5mm audio headphone.
Here is a high-level summary of some of the devices and we have newer devices in the product portfolio link below.
2318.AIC products.pdf
Audio CODECs product selection | TI.com …
You can look at this high-level summary for some of the devices. AIC3106 DMIC is on GPIO1 and GPIO2 for example which you can use but check against your requirement from the list.
7317.AIC products.pdf
Hi,
Currently we don't have codec with SRC and ClassD integrated into single IC, this will probably be next year.
We have SRC devices listed in this link below, which you can combine with codec with ClassD (see attached file) as one option.
Audio…
Hi,
I have the high-level summary of these devices but might not be to the details that you are looking for.
5543.AIC products.pdf
Datasheets will still be the place to get that.
In AIC3268, the information is now in the datasheet as compared…
Hi,
These devices are with fully differential line output, you can either replace with differential to single ended or use device like AIC3204.
Here is a high-level summary of some of the codec devices.
6747.AIC products.pdf
Regards.
Hi,
I have attached here a high-level summary of the current codec devices that might meet your requirements.
Our current DSP devices have limited resources to support AEC and other algorithm, we would recommend using external DSP to run algorithm…