Hi All,
Could someone help with two questions?
1) The TLV320AIC36 can sample audio at 32 bits / 48 KHz then pass internally to its miniDSP then pass the output of the miniDSP to a host processor such as the Raspberry Pi (and reverse for audio output)?…
When phase shift between multiple codecs is a concern it is recommended to turn on the ADC before apply the WCLK/BCLK/MCLK signals. The following steps could be used as a guide: 1. Disable MCLK/BCLK/WCLK. 2. Soft reset and config registers, then write…
To start miniDSP code development, you need to:
1. Obtain an EVM:
TLV320ADC3101EVM-K TLV320AIC3111EVM-K TLV320AIC3120EVM-U TLV320AIC3253EVM-K TLV320AIC3254EVM-K TLV320AIC3254EVM-U TLV320AIC3256EVM-U TLV320AIC3262EVM-U TLV320AIC3263EVM-U TLV320AIC3268EVM…
Hi Ivan-san,
Thank you for your reply. Could you please tell me the registers that I should set to be concrete although I understood that TLV320AIC36 is able to converter the analog signal to PDM output(DSD output) ?
Best regards, Kato
Hi Nicolas,
Have you seen the TLV320AIC36? It has a dedicated ADC with configurable windows to detect and identify multiple resistance combinations.
Regards,
J-
Hi Joy,
Unfortunately, the smallest size we have for DirectPath is http://focus.ti.com/docs/prod/folders/print/tlv320aic3256.html and http://focus.ti.com/docs/prod/folders/print/tlv320aic36.html .
Regards,
J-
Hello Christian,
I understand your concern. THD, SNR, amplitude and response should be similar when both are driving line loads. Coloration is mostly due because of response and/or THD differences.
You might also want to take a look at our other miniDSP…