Hi, Shani,
I'm not sure I understand what you're looking for.
We have parts like TLV320DAC23 that do I2S to HP-out.
But, it requires some I2C or SPI programming to set up some registers.
I guess that you are looking for an IC that does this without…
Yep, the TLV320AIC23B IPWRG4 is the one. The TLV320DAC23 is a DAC, not a codec.
The TLV320AIC23EVM2 has the codec and DAC on the same board, but I'm checking to see if a USB adapter is necessary. They would also have to jump off the IC pins to get to…
Dear sir
I am doing a project that requires a codec IC. and I have chosen to use a TI part TLV320AIC3204 . But at the same time I also found TLV320DAC23 .
can anyone tell me what exactly is the different between above two ICs?
Awaiting for the fruitfull…
Other Parts Discussed in Thread: TLV320AIC3204 Dear sir
I am doing a project that requires a codec IC. and I have chosen to use a TI part TLV320AIC3204. But at the same time I also found TLV320DAC23.
can anyone tell me what exactly is the different…
Other Parts Discussed in Thread: DSD1608 , PCM5100 Hi,
I'm new on audio device, and tryng to add to a beagleboard tree audio output.
Beagleboard have a McBSP on expansion port, but in the DSD1608 I see more than one data in (seems a McASP),
can I…
Hello Vikas,
I disabled these bits because according to the application note 'Dynamic Behavior of the TLV320DAC23 and the TLV320AIC23B' if OSC is disabled, MCLK still functions. And regarding to the CLK bit, it powers off the CLKOUT pin because we don…
Other Parts Discussed in Thread: TVP5158 Hi,
My system configuration consists of the following:
DM6467 900 MHz, 256 MB DDR2 400 MHz
TVP5158 configured to send 4 D1 (line interleaved) to DM6467 + 4 mono audio inputs (8kHz)
tlv320dac23 configured to output…