Part Number: TLV320DAC3100 In the datasheet for the TLV320DAC3100 , Figure 4-7 shows an FFT plot of the system producing a sine wav at full scale. I am interested in this figure because it shows the noise floor vs frequency.
Unfortunately, I cannot…
Part Number: TLV320DAC3100 In a similar vein to this thread TLV320DAC3100: LTC and Revision Change , we also suspect a behaviour change on a recent batch of TLV320DAC3100.
It appears that the Vrms level from the SPKR is lower than it was (using the…
Part Number: TLV320DAC3100 Hello,
Can you confirm if the TLV320DAC3100 should have a solid ground plane or split ground plane. The datasheet recommends a split plane, joined "in a few points". The eval board has a single, solid ground plane.
Which…
Part Number: TLV320DAC3100 Other Parts Discussed in Thread: TPA6166A2 Hello,
Is there a recommended EMI filter for the headphone output of the TLV320DAC3100?
The TPA6166A2 datasheet recommends a pi filter with 33pF shunt caps, and a 22R @ 100MHz ferrite…
Part Number: TLV320DAC3100
Hi all,
We are planning to support 192 kHz / 32-bit operation.
For 4-channel TDM operation, we believe the BCLK needs to be set to 24.576 MHz .
However, with this BCLK frequency, the high time and low time of BCLK are…
Part Number: TLV320DAC3100 Dear TI Team,
Excuse me!
Please find attached information regarding a suspected application issue recently encountered by our company. ABA cross-verification indicates it is related to failed ICs, but no defects have been…
Part Number: TLV320DAC3100 Other Parts Discussed in Thread: TAS2572 I am designing a wearable/TWS device with a strict 130mAh battery and a maximum 4x4mm PCB footprint. I need an I2S digital-input amplifier (or DAC) with ultra-low power consumption and…
Part Number: TLV320DAC3100 Hi TI Team,
Urgent.
TI MPN: TLV320DAC3100IRHBR to refer.
Please help to advise if any revision change for this particular item?
If yes,please provide the details.
Hi Kathy,
Please help to advise if TI have in stock…