Part Number: TLV320DAC3100-Q1 Hi team,
I would like to reduce communication commands between MCU and TLV320DAC3100-Q1.
Besides auto increment feature, is there any way to skip duplicated command such like sending the device address every time?
For example…
Part Number: TLV320DAC3100-Q1 Other Parts Discussed in Thread: TLV320DAC3100 Hi team,
I want to diagnose Reg.29 Overflow Flags and Reg.44 FAC Interrupt flags.
Could you advise the way to intentionally generate those flags in my board?
regards,
Part Number: TLV320DAC3100-Q1 Hi team,
What is the PWM frequency of the Class-D output amplifier of TLV320DAC3100-Q1?
Does it output the PWM signal even if no signal input?
regards,
Part Number: TLV320DAC3100-Q1 Hi team,
I would like to know the delay variation from setting 0x47 D7=1 to PWM signal output from SPKP/M terminal.
I found the thread explain it to be about 10x BCLK + additional 5ms for DAC unmute.
Does it mean the beep…
Part Number: TLV320DAC3100-Q1 Hi team,
I have a question about the sequence of Enabling Beep Generator (Reg.0x47 D7) and its configuration(0x48, 0x49....0x4F).
When I sent beep enable command (0x47 D7=1) first and then send command to set its length,…
Part Number: TLV320DAC3100-Q1 Hi team,
I am investigating TLV320DAC3100-Q1's fault(error) detection and recovery functions.
So far I could only find following items listed in status register.
Does this device have other safety mechanism such as Under…
Part Number: TLV320DAC3100-Q1 Other Parts Discussed in Thread: TLV320DAC3100 , , DRV2511-Q1 Hi team,
Could you advise the ESD structure of the TLV320DAC3100 pin31 /RESET?
TLV320DAC3100-Q1 on my board was broken and it seems pin2(EN) is damaged by EOS.
…
Part Number: TLV320DAC3100-Q1 Hi team,
I have a question about power up sequence of TLV320DAC3100-Q1.
I designed all the power rail to 3.3V (SPKVDD, HPVDD, IOVDD, AVDD) except VDD=1.8V, and configured to power up all rails at the same time.
It is not…
Part Number: TLV320DAC3100-Q1 Hi team,
I am trying to utilize Beep generation function of TLV320DAC3100-Q1.
The only clock I supply to this chip is MCLK, but I found the other e2e thread explaining that the Beep generation function requires
at least…
Part Number: TLV320DAC3100-Q1 Other Parts Discussed in Thread: TLV320DAC3100
Hi Team,
My customer would use TLV320DAC3100-Q1 for automotive cluster application, and need drive 50ohm speaker.
Could you help check and suggest if TLV320DAC3100 could drive…