Part Number: TLV320DAC3101 Hello team,
Could you please address SW questions from my customer?
Does TLV320DAC310x support Linux driver and has reference code? I found this should be OK from the other thread, but I want to double check here.
Is…
Part Number: TLV320DAC3101 Dear Team,
Our customer have a question as below, could you help to support it?
Customers generally use i2S signal input, the clock signal is also normal, but HPL and HPR output is only 1.2V. Could you guide us how to…
Part Number: TLV320DAC3101
Hello E2E,
The TLV320DAC3101 has a power sequencing regulation from the Rev-B data sheet. However, that doesn't match past E2E answer. e2e.ti.com/.../2324485
1: Which is correct about power up sequense, Rev-A or Rev-B…
Part Number: TLV320DAC3101 Other Parts Discussed in Thread: TLV320DAC3203 , TPA6017A2 , TLV320DAC3100 Hi, TI team,
The TLV320DAC3101 integrates two class-D speaker drivers.I know it can driver two differential loads(SPLM/SPLP、SPRM/SPRP) . But my custom…
Part Number: TLV320DAC3101 Hi sir,
Could you help to check how do we connect unused pins as highlighted yellow in below?
We only use the speaker function on SPLM/P through I2S.
Thank you.
Part Number: TLV320DAC3101 Hello,
I would like you to confirm whether following description is correct or not.
* 1: Beep generator is enabled (self-clearing based on beep duration).
According to confirmation w/ CodecControl and DAC3101 EVM, when…
Part Number: TLV320DAC3100 Other Parts Discussed in Thread: TLV320DAC3101 , TLV320DAC3120 My customer currently uses the TLV320DAC3100 in the circuit. If replacing it with the TLV320DAC3101 in the same PCB, will any issues occur? The main concern is with…
Part Number: TLV320DAC3101 We use AM3558 with linux and our device emits of spurious emission when the class D is on
Is there a command in the user space to put the class D off (page 1 register 0x20 value 0x6)?
we cannot output I2C command since the…
Part Number: TLV320DAC3101 Hi,
I have questions about I2C timing specifications of this device. Please tell me about described below.
About tHD;STA, tSU;STA, tSU;STO.
These specifications in Fast Mode are "min. 0.8us" described in the datasheet…