Part Number: TLV320DAC3120 I'm working on an application with the '3120 that uses the converter, routing and speaker amp, but doesn't use any filters are other dsp functions. What register configurations will provide the lowest power operation?
Thx…
Part Number: TLV320DAC3120 Other Parts Discussed in Thread: TLV320DAC3203 , TPA2013D1 , TAS5411-Q1 Hi,
We are using TLV320DAC3120 DAC in our project. We are using a 0.8W and 8ohm speaker at its output. But as the speaker performance is not good, so…
Part Number: TLV320DAC3120 Dear All,
We are using the TLV320DAC3120 chipset in our project.
We have tested the below sampling rates and we haven't faced any issues.
8 kHz
16 kHz
32 kHz
44.1 kHz
48 kHz
But when we are playing 22.05KHz…
Hi, Thorben,
Welcome to E2E and thank you for your interest in our products!
You are right, there are some recommended delays that you should consider in your design in order to have the device properly initialized. As mentioned in sections from 5…
Part Number: TLV320DAC3120 Hi Audio team!
I would like some assistance in figuring out the lowest power I2C settings that I can put the TLV320DAC3120 in. The need is for no miniDSP use but just the I2S data through the DAC and output the Class-D speaker…
Hi, Twittich,
Thank you for providing the details in the pictures.
The PLL configuration is correct for the clocks that you are using. Regarding the data from DIN, it seems that you are sending the data through the right channel (see I2C configuration…
Part Number: TLV320DAC3120 What is the input resistance of AN1 and AN2 in TLV320DAC3120? If not resistive, please provide detail on input impedance vs. frequency. Thx.