Other Parts Discussed in Thread: TLV333 Hi team,
Could you help to explain the short circuit current means?
My customer want to know the short circuit current at -20 & 120 degC. Do you have the data?
Thanks
Other Parts Discussed in Thread: TLV333 Hello,
Our customer uses the TLV333, has an issue.
The customer are using the TLV333 as follows.
circuit : non-inverted amplifier
VCC=3.4V
amplitude : 261 times
pre-filter : RC low pass filter as R=10kohm, C=1uF…
Hello Robert,
We have explored several reference designs, but the presence of numerous discrete components in the circuits is not ideal for our requirements.
We received valuable guidance from @Art & @Raymond from the Precision OpAmp team, suggesting…
Other Parts Discussed in Thread: TLV333 , TINA-TI Hello,
Our customer said TLV333 has bad temperature drift in simulation, so I had tried TINA-TI simulation with sbom966 on the web.
The result was 40uV/degree, it is too big against typical value 0.02uV…
Part Number: INA333 Other Parts Discussed in Thread: OPA391 , TLV387 , OPA333 , TLV333 , OPA387 , OPA187 Hello
I designed sEMG PCBA with INA333 as first stage of amplifier,first time I used the same SCH as bellow,and the ouput signal is correct.
The secon…
Other Parts Discussed in Thread: TLV333 Dear Specialists,
My customer is considering TLV333.
He is some questions about chopper frequency.
Could you please advise?
(1) What hertz is the chopping frequency?
According to the datasheet, 8.3.3 Internal Offset…
Other Parts Discussed in Thread: TLV333 , OPA333 , INA333 I am looking for a precision opamp with low supply current for precisely sensing currents in the range of 0-10 uA on a -60 V rail. The opamp would be powered by shunting some current from this rail…
Dear Marek,
Thank you for your reply.
How about TLV333? it has 0.015mV offset voltage and 0.02uV/C offset drift. It is little worse than OPA387, but I want to know it is good to use or not. (because it would be easy to get TLV333.)
and do you have any…
Other Parts Discussed in Thread: OP07 , TLV2470 , TLV333 , OPA396 I am looking for a precision amplifier that can support the following conditions:
Vin: 5mV – 10mV (DC Voltage)
Single supply of 3.3V.
Vout: ~0.5V.
The voltage ripple (p-p 250uV) will…