Hi Taylor,
TLV3401 is one part of Amplifiers and linear portfolio. The engineers who answer questions in Amplifiers & Other Linear Forum are experts in TLV3401.Please ask help from 'Amplifiers & Other Linear Forum'.
Thanks
Lawrence
Other Parts Discussed in Thread: TLV3401 In TLV3401 datasheet, I have seen a diagram on page 1, showing volatge divider with two 1Mohm resistors. How much maximum value of resistor I can select like if I go to 2Mohm each. What limits its value?
Other Parts Discussed in Thread: TLV3401 The TLV3401IDBVR is an open-drain output comparator, but the data sheet does not give any specifications for the max drain-source voltage for the output stage.
Question 1 -- Is the maximum output drain-source…
Fethi,
The TLV3404 is a quad device in a product family that includes the single-channel version, the TLV3401. They will share the same model; it was an oversight on our part for not making the model available on the TLV3404 product page. The TLV3401 Orcad…
Other Parts Discussed in Thread: TLV3401 , TINA-TI Hello,
I am trying to build a simple circuit that can detect whether a conductive nanoscale cantilever probe (basically, a sharp needle) is touching a bare Au substrate. Currently, I have used one of TI…
Other Parts Discussed in Thread: TLC374 , TLC339 , TLV3401 , TLV3701 Dear support,
I am looking for the value of the input parasitic capacitance for both the TLC339 and TLC374 - this is not shown in the documentation
Thank you - Yves Camille - Arrow El…
Hi Alexander,
I was traveling this past week and I am still catching up on email.
It is difficult to know what the problem could be without having all the circuit details. They mention the inputs being about 500 mV apart and coming up with Vcc, but then…
HI Zachary,
The common mode limit is an absolute for each pin, not the average of the two pins. The formula is correct, but not applicable...
Comparators can have differential voltages of several volts, so one input does not get a "free-pass" because…
Hi,
I have now used two TLV3401. Below is the schematic:
Problem is when no current flows U2 is high but U1 gives o/p low. I don't understand why this happens? I checked voltage at inv & non-inv terminal of U1, volatges are same. Then why there…
Other Parts Discussed in Thread: TLV3501 , TL3016 , TLV3401 , TLV3701 , TL712 , LM306 , OPA836 what is the high speed performs regarding of low speed input ? In my understanding the output will be instable esp. near the threhold point. it is the second time…