Hi Mohammed,
While I will continue to recommend OPA310 when it gets stocked, since it's the newest and has the best specs, I think the TLV341 would be a good alternative, though it's right at the edge of the 100mA requirement. The LMV861 would likely…
Hey Sakuma-san,
I recommend transitioning to a low voltage device, specifically the TLV341 in the DRL (SOT-5X3) device.
https://www.ti.com/product/TLV341#order-quality
We currently have a lot stock available on ti.com
Also if the highest priority is…
Part Number: UC3845 Other Parts Discussed in Thread: TLV341 , TL431 , , UC3842
High ripple on the output voltage?
Hi dear team, I made a switched mode power supply circuit using UC3845. And I made the circuit on the lab using flyback transformer from…
Part Number: OPA170 Other Parts Discussed in Thread: TLV341 , OPA171 , OPA990 Hi, Staff
Customers are currently using OPA170 SOT-5X3 (DRL Package). We are planning to revise the application, but we will not change the board layout.
Customer demands are looking…
Hi Nesh,
The capacitor increases the high frequency gain of the control loop by providing a low impedance path for high frequency signals around R12.
I would use the TLV341 with a 1.24V reference. The TL431 is a 2.5V reference and when used with a 3.3V…
With a low supply voltage, then I recommend the OPA341 or TLV341. Both will be better choices than the LM321 and have more output current drive. They are also pin to pin.
-Paul
Part Number: OPA313 Other Parts Discussed in Thread: OPA322 , LMV951 , TLV341 , TLV341A Hi,
My customer would like to know the absolute minimum supply voltage for the below parts. Datasheet shows 1.8V to 5.5V recommended operating range but they are using…
Hi Ron
Thank for your reply.
What i was expecting, was to get a variation in voltage as my EC or resistance between probes was to change.
Yes i am seeing a nice clean 43.201 Khz output , when input is the same.
So as EC changes should i see a variation…