Part Number: TLV3691 Other Parts Discussed in Thread: TLV7031 , TLV7081 I am making a circuit using the TLV3691 nano-power comparator using VCC = 3.3V. I want to connect one of the inputs directly to VCC. The other input is connected trough a 2 MEG resistor…
Part Number: TLV3691 Hello,
The maximum Ibias shown in the data sheet is 20 nA across the full temperature range. In my application the allowable temperature range is -40C to 85C. I would like to find out if there is any data indicating the maximum Ibias…
Part Number: TLV3691 Hi,
I have a small issue with the comparator that I am designing.
I want to monitor the voltage on my capacitor using the TLV3691 such that when the caps are charged to 12.5V, the output pin should be low and when the caps are discharged…
Part Number: TLV3691 Hi team,
My customer is using the TLV3691 as a comparator to monitor the voltage from a Potential transformer (PT). The negative input of TLV3691 is connected to the PT output and the positive input of TLV3691 is connected to a reference…
Hi Neil,
No it hasn't been fixed, but the model is scheduled for the work. I just checked the modeling group's schedule and it shows a forcasted date of 06/29/17. Please note that all the TI analog comparators, including the TLV3691, are now supported…
Other Parts Discussed in Thread: LM8365 , TLV3691 , LMP7300 , REF1112 , TPS3839 Hi E2E,
I'm trying to make an ultra-low-power voltage supervisor with discrete parts (comparator, voltage ref...) for a customer.
I'm coming from this E2E post which looked…
Other Parts Discussed in Thread: TLV3691 , TLV3702 , TLV3492 , LPV802 , TLV8802 , SN74LV1T34 Hello,
I'm looking for exactly what's in the subject line -- a dual version of the TLV3691 comparator. Based on the parametric search, it doesn't look like…
I have also doubt in this part. N mosfet cannot pass positive voltage from drain to source completely (not strong one). N -Mos will drop Vgsth across source and drain. But if we use a P mos instead of N mos it can pass positive voltage completely from…
Other Parts Discussed in Thread: TLV3691 Will it damage the device to temporarily have the TLV3691 inputs at a higher voltage than VCC? I am using the comparator to monitor battery voltage but have it powered from the regulator output. When batteries are…