Hi Ben,
Yes, that's a valid use case, but it will take a slightly more creative solution. One more question, will IN1 be dropped to a lower voltage during operation, or will it just be connected/disconnected?
What do you think about something like…
Hi Eva,
thanks for the further inquiry.
I just want to know a capacity range, where the HLDO_OUT is stable.
But for now i derived my design from your examples in figure 8-1 and 8-5 in the datasheet and i only added a reference shunt diode (TLV431AID)…
Part Number: TLV431 Other Parts Discussed in Thread: TLVH431 I am looking for an Low-Voltage Adjustable Precision Shunt Regulator like TLV431 with reference voltage from 0.5V to 16V.
Part Number: UCC256301 Dear Team,
I am working on PFC+ LLC for 40V,3A application for TV application.
The load regulation are pretty worse if I use EVM default compensation setting.
The output are 41V at no load but 40V at 3A load.
Adjust the compensation…
Part Number: TLV431B Other Parts Discussed in Thread: TLV431 ,
Dear team,
The customer want to get function safety certification for their application.
Currently they are using TLV431BQDBZR at their application.so they would like to know if TLV431 is Type…
Hi Lillian:
1. When testing the OUT-GND driving signal, you can use an ordinary oscilloscope probe, no need to use a differential probe. The slight whistling sound would occur when probing signal waveforms as they are more perceptible to noise when there…
Hi Walter
Thanks for the answer :-)
The two you mention are not for the 28V input that we have in your system. TLV431 max = 6V, TLV431 = 20V. What do you mean by "not working well" in comparator mode? And is it possible to get data for this mode?…
Part Number: TLV431 Hi all,
I am trying to build a constant current sink using the TLV431 as a voltage reference and a NPN BJT (BC549C) on the output.
The circuit is shown below:
VG1 is the PWM signal (0-5V nominally), AM1 is used to monitor the current…
Part Number: TLV431 Other Parts Discussed in Thread: TINA-TI , , OPA333
Tool/software: TINA-TI or Spice Models
Hi team,
My customer is using TLV431 in their project. And they use TINA-TI to simulate it. We can get from TLV431's datasheet that the output…