Part Number: TPS23770 Other Parts Discussed in Thread: TPS23750 , TPS23750EVM-107 , TLV431
I modified the circuit on page 33 with a different switching mosfet and a different diode. For some reason I'm getting 38V or 40V on the output. I did my own layout…
Hi,
The application note uses TLV431, and if you read the associated content, the note mentions a ref of TLV431 is 1.24V.
Vopto is 15V if you connect it to 15V.
Part Number: TL431 Other Parts Discussed in Thread: TLVH431 , TLV431 Hello All ,
I am using TL431 as a switch to turn on /off logic level MOSFET.
When the input voltage is above internal reference voltage , 'VKA _low' voltage is around 1V for TLV431…
Other Parts Discussed in Thread: TLV431 Customer has a TLV431 part with the part marking "YAIL". Can you tell me if the part markings is for TI voltage ref part TLV431CDBVR or TLV431AIDBVR? Both of these two parts are listed on the AVL so the c…
Hello Tanaka-san,
This is an older device and there is no dedicates model. This is the closest alternative:
https://www.ti.com/product/TLV431?keyMatch=TLV431&tisearch=search-everything&usecase=GPN#design-tools-simulation
Thanks.
Part Number: TL431 Other Parts Discussed in Thread: , TLV431 , ,
What is the recommended operating condition for refernce pin of shunt regulators { TL431/ATL431/TL431LI/ATL431LI/TLV431/ATL431LI}?
Other Parts Discussed in Thread: TLV431 Hi,
The datasheet for the TLV431 specifies different min/max values for the device depending on the temperature grade (C/I/Q). I have two questions:
What happens to the industrial device (-40 to +85C) if it is operated…
Other Parts Discussed in Thread: TLV431 Hi,
Considering that the maximum Cathode-Anode voltage from TLV431 is 6V, could it regulate from 24V to generate 5V output voltage using a typical application circuit (similar to datasheet's Figure 2)?
Is there…
Part Number: UCC2891 Other Parts Discussed in Thread: TINA-TI Hi Experts,
I am looking to design a 300W DCDC converter with the following specs:
Vin = 70VDC- 125VDC
Vout = 9VDC-16VDC, 14.4VDC nominal.
pout = 300W
isolated topology
I came across this…