Part Number: TLV5627 Other Parts Discussed in Thread: DAC5573
Hi app specialists
I am finding Ti device that alternative from ADI AD5306ARUZ.
So could you tell me what kind of device is the best for us.
if you tell me, also could you tell…
Hello Uttam, thanks for the welcome.
UPDATE:
Yesterday I managed to solve my issue with the TLV5627. The SPI clock polarity I was using was incorrect.
The correct SPI Clock polarity is:
Idle state: HIGH
Active state: LOW
The (Incorrect…
Other Parts Discussed in Thread: TLV5627 8-bit 4-channel DAC TLV5627 is used in our product. And our product is used in field of building automation. We found that sometimes the TLV5627 in our product will enter a weird "Locked" status, that is:
Whatever…
Part Number: ADS1258 Other Parts Discussed in Thread: TLV5627
Hi Team,
Our customer noticed that when the input voltage to AIN5 pin of the ADS1258 is 0V the measured voltage is not zero ( 0x00020A70 - which is a count of 133,750). According to our…
Hi Chen,
Thank you for your query. The maximum update rate possible with DAC104S085-Q1 is 1.8MHz in the worst case 1/(t_SYNC+t_SS+t_CFSR). If we divide that by 4, we get an update rate of 453kHz per channel assuming separate writes per channel. Now…
Sai Loo,
According to the Qualification report, the TLV5627 was qualified together with the TLV5604 and TLV5614. The ESD passed 4000V HBM, 400V MM, and 1500V CDM. The qual is dated to 3/00.
Joseph Wu
Part Number: TPS63020 Other Parts Discussed in Thread: TMS320F2812 , TIDA-050017 Hello Expert,
I have already requested about Quad-Channel TEC Controller on CSC.
So I got a feedback as below my case #.
CS1305244
Our customer is finding Quad-Channel…