Part Number: TLV5638 When our product main power is turned on, the reference voltage is intermittantly outside of the reference accuracy tolerance for this device. This issue is occurring only on TLV5638CD devices with a Package Marking of TI 57T ASNX…
Part Number: TLV5638 Tool/software: Hi,
I would like to know the recommended decoupling capacitors.
According to document SLAA113A, a 4.7uF electrolytic capacitor and a 0.01uF ceramic capacitor are used.
Is it recommended to use an electrolytic…
Part Number: TLV5638-EP
Hi,
I want to know the timing constraints for continuous access.
How long between 1st /CS rising edge and 2nd /CS falling edge is needed?
We can not find the time in datasheet.
I am looking forward to hearing from…
Part Number: TLV5638 I have connected PIC 18F6520 Microcontroller output to DAC DIN, SCLK and CS. All inputs are coming correctly, when analysed on the oscilloscope. I am first giving an output of 0XD002 for programming with internal reference of 2.048V…
Part Number: TLV5638 Hi team,
I would like to see if REF input is 2.5V, VDD should be greater than 4V. But, my customer saw, with VDD=3.3V, TLV5638 can also output 2.5V range. How to understand the relation between REF input range and VDD supply voltage…
Part Number: TLV5638 Dear team:
One of my customer use SPI which simulated by the McBSP module of f28335 to communicate with TLV5638.
Now TLV5638 chip can output DA signal normally, but there is a problem: outa and outb, only one output can be selected…
Part Number: TLV5638 Customer is reporting this:
Specifically, we are talking about the TLV5638. So far, we have installed the component on a good 10k boards. As it looks, it can happen that the reference is changed from external to internal from time…
Part Number: TLV5638 I am working on DAC tlv5638.
I am driving the sclk, cs and data from FPGA to DAC. For FPGA output i have checked it on ILA .Then I have connected the outputs from FPGA to DAC inputs. I have checked the DAC pins of sclk, cs and data…
Part Number: TLV5638 My company purchased V62/03628-02XE. All parts are correctly marked with "5638ME" as per the datasheets. Under that is "52T". Some parts have "E60N" or "A4YR" on the bottom line. What do these markings mean or what is the difference…