Part Number: TLV5638-EP In your answer to the question "Need Junction to Case (Theta JC)- TLV5638-EP (V62/03628-02XE)", you gave a list of Theta-JC and Psi-JT for Low and High K boards.
However, you gave multiple, different values for each of…
Other Parts Discussed in Thread: TMS320F28335 , TLV5638 I am using TMS320F28335 DSP for motor control.
In this DSP, 4 kHz control rate is implemented by the CPU timer interrupt. And then, SCI (PC to DSP), SPI (for TLV5638), 2 QEP (to obtain motor position…
Other Parts Discussed in Thread: TLV5638 Hi,
I am making user SPI interface with TLV5638.
As you know TLV has two DAC channels.
Using three of GPIO of 320F2801-60 I made an interface to communicate with TLV.
It seems that it is working well when I only…
Other Parts Discussed in Thread: TLV5638-EP Hi!
We are using the TLV5638-ep, powered with 3.3 V. The datasheet states that the 2x output is rail-to-rail, but in the output specifications (data sheet page 5) the output voltage is stated to be max Vdd-0…
Other Parts Discussed in Thread: TLV5638 We have using Serial DAC TLV5638C in our system for more than 5 years without issue.
Recently we have been seeing an accuracy issue with the internal reference at power up on a few devices (occurring on about 5…
Other Parts Discussed in Thread: TLV5638 We are driving the TLV5638 with an Atmel ATTiny controller. We cannot get the SPI interface to work. We have to write the command twice in order to get anything out. Looking at the data transfer with a scope shows…
Other Parts Discussed in Thread: TLV5638-EP Hi Can you please provide the following information for the TLV5638-EP (V62/03628-02XE) Part ?
Thermal Resistance Junction to Case (Theta JC)
Other Parts Discussed in Thread: TLV5638 Dear Friends,
I am using PIC32 and tlv5638. I have checked waveforms on DSO. it is ok. So I thing I am missing some configuration tlv5638. I want to use both the channels.
I am not able to see variation in analog…
some primer of working code for TLV5638 (avr asm):
;=================================================
; Initialization 5638 >
;==================================================
cbi SPSR,0; SPI X1
in resTemp,SPCR;
…
Part Number: TLV4316 help me,urgent,Consult Ti chip design engineer or chip processing engineer,Whether there is ti logo in the internal layout of TLV4316 chip.
The following is the internal logo identification of TLV5638 chip for reference.