Part Number: TLV61047EVM Other Parts Discussed in Thread: TLV61047 Hello,
I'm using the TLV61047 evaluation kit and I updated R_FBB to 47k and R_FBT to 1M in order to have an output voltage just below 28V. The output voltage was then measured to 27…
Part Number: TLV61047 Inquiries about the TLV61047DDCR
■Setting Conditions VIN: 12V VOUT: 16V (Design Value) Load Conditions: 30mA (Max)
1. Up to what load current can the SW pin output voltage maintain the switching frequency (1.6MHz (TYP) pulse…
Part Number: TLV61047-Q1 My application is 2.8Vin & 8Vout at 0.4A. I am interested to know the power dissipation of the IC. The datasheet's efficiency data shows total loss but kindly help to estimate the power dissipation of the IC. For earlier designs…
Part Number: TLV61047 Other Parts Discussed in Thread: TPS61378-Q1 Dear TI experts,
My customer is looking for a boost converter which meets the conditions below;
Input voltage : 6.4V~8.4V (2S Li-ion battery)
Output voltage : 12V
Output current…
Part Number: TLV61047 Tool/software: Hi TI team,
We are designing a circuit using the TLV61047 to drive a LCD Backlight and would appreciate your help reviewing our schematic for any potential issues.
Part Number: TLV61047 Other Parts Discussed in Thread: LMR64010 Tool/software: Hi All,
I have a question about the TLV61047 and LMR64010.
Do these two products have built-in phase compensation circuits?
The datasheet mentions "internal compensation…
Part Number: TLV61047 Tool/software: Hi All,
I have a question about the TLV61047.
(1)When I performed the calculations according to 8.2.1.2.2 Inductor Selection, the inductor was 120uH. VIN=12,VOUT=17V,IOUT=30mA However, it states that the recommended…
Part Number: TLV61047 Tool/software: Hi,
I can't find TLV61047DDCR from Find Product by Package | Texas Instruments and MTBF and FIT Rate Estimator , but this device has already RTM'd.
Could you help to add TLV61047DDCR into the system?
Thanks.
Part Number: TLV61047 Tool/software: Hi TI team,
We are designing a circuit using the TLV61047 to drive a 10V motor and would appreciate your help reviewing our schematic for any potential issues.
Thanks!
Part Number: TLV61047 Tool/software: Hi All,
I have a question about the TLV61047.
Is there any documentation showing the accuracy of the output voltage?
For example, It can output 15V with an error of ±3%.
I would like to know the 15V output…